×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 64906050, Entry date: 04/08/2019
(16)
Rate

Creation of report templates for the Information Server based on Process Historian data in the WinCC and PCS 7 Environment

  • Entry
  • Associated product(s)
World-wide competition, increasing energy costs, scarce raw materials and high demands to product quality – companies from the process industry face many challenges. Specific optimization in view of process excellence and profitability are a must.

Task  
Historic data from the company is a key to increase productivity. In order to make this enormous amount of data accessible for plant optimization, a powerful archive and report system is required.

The following requirements should be fulfilled:

  • availability and security of data
  • aggregation of information that is relevant to process control due to cross-company production report systems
  • central archiving of process data, tags, alarms and batch data from SIMATIC BATCH in realtime and without requiring additional energy as well as seamless, long-term and reliable data capture
  • identification and memorizing added and modified data as audit trail information
  • task-specific reporting and visualization of data
  • powerful data export to Microsoft Excel
  • flexible creating and adjusting report templates
  • standard reporting systems, in order to be able to use already available expert knowledge

Solution  
This application describes the basics and the principle of operation of the Process Historian (PH) and of the Information Server (IS). It will be explained in detail how you can create individual reports in order to be able to read out data promptly from the Process Historian database. Furthermore, you will learn how to work with the Process Historian database.

Core contents of this application example:

  • explanation of the basics and of the function principle of the Process Historian
  • description of the Report Builder (tool for creating reports)
  • correct working with the PH database
  • explanation of the Stored Procedures of the Process Historian
  • prepared and described report templates for download

The Process Historian (PH) and Information Server (IS) have, among others, the following functionalities and benefits:

  • All OS process data is promptly available in the process historian.
  • Batch archives of SIMATIC BATCH are saved natively in the process historian.
  • PH also supports single stations.
  • PH supports several PCS 7 / WinCC projects in parallel.
  • Easy access to historic process data via web and office applications.
  • Widely used standard reporting system that is adjusted to PCS 7 / WinCC reporting incl. standard reporting templates.
  • PH can be easily integrated into existing IT infrastructures and web portals.
  • Large volumes of process data can be prepared and displayed in reports across projects.
  • With WinCC Trend and Alarm Control data from PH can also be displayed on the OS Runtime level.
  • With OPC HDA / "H A&E" PH data can be accessed.
  • Backup/restore function on external data carriers.

Validity

Complete package of all templates with documentation
 Registrierung notwendig   Registrierung notwendig Complete package of all templates with documentation (418,3 MB) (418,3 MB) 

Creation of report templates with the Report Builder
  Documentation (3,5 MB)   
 Registrierung notwendig Prepared report templates (16,1 KB)

Creation of report templates with the Report Designer (Visual Studio)
 Documentation (2,8 MB) 

Report template: APF with WinCC User Archives in the PCS 7 environment
 Documentation (2,1 MB)

Report template: Report for database administrators and service personal
 Documentation (1,0 MB)
 Registrierung notwendig Prepared report templates (38,8 KB)

Report template: Analysis of APL PID controller characteristics
 Documentation(1,1 MB)
 Registrierung notwendig Prepared report templates (9,0 KB)

Report template: Advanced message reports
 Documentation (1,9 MB)
 Registrierung notwendig Prepared report templates (26,1 KB) 

Report template: Process Operation Report
 Documentation (913,0 KB) 
 Registrierung notwendig Prepared report templates (6,6 KB) 

Report template: Creation of a report with logon and logoff information for PCS7 OS
 Documentation (1,0 MB)
 Registrierung notwendig Prepared report templates (6,2 KB)

Report template: Frequently filtered entry lists
 Documentation (987,0 KB)
 Registrierung notwendig Prepared report templates (7,9 KB)

Report template: Valve switching
 Documentation(1,2 MB)
 Registrierung notwendig   Registrierung notwendig Prepared report templates (14,0 KB) (14,3 KB)

Report template: APL Symbolblock note report
 Documentation (2,1 MB)
 Registrierung notwendig Prepared report templates (13,0 KB)

Report template: Configurable trend report for variable intervals
 Documentation (1,4 MB)
 Registrierung notwendig Prepared report templates (4,9 KB)

Report template: Aggregation of variables

 Documentation (2 MB)
 Registrierung notwendig Prepared report templates (14,7 KB)

Report template: Reading-out aggregated tables of the Process Historian
  Documentation (1017,8 KB)
 Registrierung notwendig Prepared report templates (7,0 KB)

Report template: Advanced Tablix Report
 Documentation (1,5 MB)
 Registrierung notwendig Prepared report templates (28,0 KB)

Report template: Generation of report templates for diverse SFC types

 Documentation (1,3 MB)
 Registrierung notwendig Prepared report templates (27,0 KB)
 Registrierung notwendig Exemplary project (363,2 MB)

Report template: Recording of motor runtimes
 Documentation (857,7 KB)
 Registrierung notwendig Prepared report template (5,3 KB)

Report template: Trend for two variables with secondary Y-axis

 Documentation (945,1 KB)
 Registrierung notwendig Prepared report template (5,7 KB)

Report template: Output of messages with SIMATIC BATCH names
  Documentation (706,9 KB)
 Registrierung notwendig Prepared report template (8,7 KB)

Report template: Usage of report templates for alarm statistics
 Documentation (1,2 MB)
 Registrierung notwendig Prepared report templates (41,8 KB) (57,1 KB)

Report template: Message-Associated Value Report
 Documentation (1,1 MB)
 Registrierung notwendig Prepared report templates (19,6 KB)

Report template: Use of singal status report templates
 Documentation (729,6 KB) 
 Registrierung notwendig Prepared report templates (11,0 KB)

Report template: Representation of variables and messages over a time range
 Documentation (1,4 MB)
 Registrierung notwendig Prepared report templates (15,7 KB)

Report template: Message cycle report for the information server
  Documentation (941,1 KB)
 Registrierung notwendig Prepared report templates (11,3 KB)

Report template: Single message report for the information server
  Documentation (694,8 KB)
 Registrierung notwendig Prepared report templates (7,8 KB)

Report template: Dashboard report for the information server
  Documentation (1,7 MB)
 Registrierung notwendig Prepared report templates (46,6 KB)

Report template: Tabular SIMATIC BATCH report for the information server
 Documentation (1,4 MB)
 Registrierung notwendig Prepared report templates (22,5 KB)

Report template: Use of SIMATIC BATCH report templates with the information server
 Documentation (941,2 KB)
 Registrierung notwendig Prepared report templates (16,4 KB)

Report template: Trend comparison for one variable and two time ranges
 Documentation (886,9 KB)
 Registrierung notwendig Prepared report templates (8,7 KB)

Report template: Displaying a data matrix with selectable variable cycle
  Documentation (781,8 KB)
 Registrierung notwendig Prepared report templates (5,4 KB)


Further information
SIMATIC Process Control System PCS 7 Readme V9.0 (Online)
WinCC V7.4 SP1: General information and installation  
SIMATIC Process Historian 2014 SP3 
SIMATIC Information Server 2014 SP2
Installation, Operation and Maintenance of PH/IS in a PCS 7 environment

Last changes
The report template "Displaying a data matrix with selectable variable cycle" was added.
The "Complete package of all templates with documentation" includes the newly added report template.