×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 65358096, Entry date: 11/09/2012
(0)
Rate

Why is it possible that the temperature range specified on the device rating plate on SIPLUS modules differs from the temperatures specified on the data sheet?

  • Entry
  • Associated product(s)
According to the UL/FM/ATEX approvals it is necessary to adapt the temperature class of SIPLUS extreme to the temperature class of BasedOn in order to extend the field of application compared to BasedOn and enable a 1:1 exchange.

Description
The data sheets include the approved operating temperatures. The figure below shows an excerpt from the data sheet of the module SIPLUS S7-300 CPU 315-2PN/DP (article no.: 6AG1315-2EH14-7AB0).

From the technical point of view, this product is released for the temperature range of -25°C to +70°C, which is also specified on the delivery documents, for example.
 


Fig. 1

Note
The temperature restriction is only necessary for applications that have to meet the UL/FM/ATEX requirements.

With these products the approved temperature range must be specified on the rating plate.

  • Here it is always the most restrictive range that is relevant for the approval.
  • This is usually the UL approval and so the temperature specification is part of the UL label.
  • In this example then it is the specification of the maximum temperature of +70°C that is reduced to +60°C.

For use at high altitudes the restrictions according to the "Extended ambient conditions" are valid (Fig. 1).
 


Fig. 2

The table below gives you an overview.
 

up to 2000m above sea levelup to 3500m above sea levelup to 5000m above sea level
Tmax
(from the technical point of view)
+70°C+60°C
(+70°C - 10K)
+50°C
(+70°C - 20K)
Tmax
(for UL/FM/ATEX application)
+60°C+50°C
(+60°C - 10K)
+40°C
(+60°C - 20K)

The reduction of the maximum temperature by 10K and 20K respectively is necessary, because at these altitudes the air density is lower because there are less air molecules for heat dissipation. +Therefore cooling of the module is reduced.

Further Information

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Hinweis: Das Feedback bezieht sich immer auf den vorliegenden Beitrag. Ihre Nachricht wird an die Redakteure im Online Support gesendet. In einigen Tagen erhalten Sie von uns eine Antwort, wenn Ihr Feedback das erfordert. Ist für uns alles klar, werden wir Ihnen nicht mehr antworten.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit