×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 65359466, Entry date: 11/06/2012
(0)
Rate

Update of the Preinstalled Software for SIMATIC PCS 7 Industrial Workstations with SIMATIC PCS 7 V7.1+SP4

  • Entry
  • Associated product(s)

The SIMATIC PCS 7 Industrial Workstations for SIMATIC PCS 7 V7.1 on the basis of the SIMATIC IPC 547D (new), SIMATIC IPC647C and SIMATIC IPC847C, as well as SIMATIC PCS 7 BOX on the basis of the SIMATIC IPC627C (as compact system / SIMATIC PCS 7 OS Client), and SIMATIC PCS 7 OS Clients on the basis of the SIMATIC IPC427C, are now being delivered with the SIMATIC PCS 7 V7.1+SP4 system software (preinstalled and on Restore DVD).

The table below provides more details. Before the change deadline listed in the table the systems concerned were delivered with SIMATIC PCS 7 V7.1+SP3 (preinstalled and on Restore DVD)! A subsequent exchange is not possible!
 

Device Type Order Number Product Release (FS) after the change PCS 7 Software at delivery (preinstalled and on Restore DVD) Change deadline (delivery ex factory)
PCS 7 Industrial Workstation, Type IPC547C 6ES7660-0....-2... PCS 7 V7.1+SP3 (unchanged)
PCS 7 Industrial Workstation, Type IPC547D 6ES7660-3....-1... 03 PCS 7 V7.1+SP4 (new),  for details see entry ID 65318450
PCS 7 Industrial Workstation, Type IPC647C 6ES7660-1....-0... 04 PCS 7 V7.1+SP4 (change from SP3 to SP4) 15.09.2012
PCS 7 Industrial Workstation, Type IPC847C 6ES7660-2....-0... 05 PCS 7 V7.1+SP4 (change from SP3 to SP4) 15.09.2012
SIMATIC PCS 7 BOX, Type IPC627C
(compact system and PCS 7 OS Client)
6ES7650-4A.0.-.... 06 PCS 7 V7.1+SP4 (change from SP3 to SP4) 15.09.2012
PCS 7 OS Client , Type IPC627C (HDD) 6ES7650-0RG17-0YX0 07 PCS 7 V7.1+SP4 (change from SP3 to SP4) 05.09.2012
PCS 7 OS Client , Type IPC427C (SSD) 6ES7650-0RG17-0YX1 07 PCS 7 V7.1+SP4 (change from SP3 to SP4) 05.09.2012

The SIMATIC Industrial Workstations on the basis of the SIMATIC IPC547C will not be updated to SIMATIC PCS 7 V7.1+SP4. Until the end of their sale they can be delivered with the following preinstalled software:

  • SIMATIC PCS 7 V7.1+SP3
  • SIMATIC PCS 7 V7.0+SP3
  • SIMATIC PCS 7 V6.1+SP4

Ordering data and prices

The order numbers and prices of the device types listed above have not changed because of the change in the preinstalled software and the associated change in the scope of delivery.
In the order configurators of the Industry Mall the changes resulting from the update will become effective as from November 2012.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.