×
Siemens Industry Online Support
Siemens AG
文档类型 产品通知 文档编号 65402168, 文档发布日期 2019年5月28日
(8)
评估

DRIVE-CLiQ Disclosure for measurement system manufacturers

  • 文档
  • 涉及产品
The DRIVE-CLiQ interface has been disclosed for measurement system manufacturers. Thus, rotary and linear measurement systems from different manufacturers will be provided with an integrated DRIVE-CLiQ interface in the future and can be directly connected to SINAMICS. New measuring systems from BALLUFF GmbH have been certified.

Updated  May 27th 2019

The interface conformity of the encoders in the system will be checked through tests at our Support Center and documented through the corresponding certificate.

To round off the system, we offer MOTION-CONNECT signal cables with M12 connectors which are required for encoders with DRIVE-CLiQ interface, see also 60179485.

Various general conditions must be fulfilled before you can operate the encoders on SINAMICS, SINUMERIK und SIMOTION. These general conditions as well as the currently available measurement systems are stated in the attached slide set.

This slide set will be regularly updated if further measurement systems are certified.


对统计的支持
用该功能可根据所需数量输出搜索结果的IDs (格式 .txt)

生成列表
复制URL
在新设计中显示此页面
mySupport Cockpit
相关链接