×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 66027369, Entry date: 07/02/2014
(13)
Rate

How do you do a program upload in STEP 7 (TIA Portal) V12 when the device has been configured with STEP 7 V11?

  • Entry
  • Associated product(s)

Description
The "Compatibility Mode V11" must be opened if a program upload of a device configured with STEP 7 (TIA Portal) V11 (a SIMATIC controller, for example) is to be made in STEP 7 (TIA Portal) V12. However, this is only possible if a STEP 7 (TIA Portal) V11 project is open.

For the case that you do not have a STEP 7 (TIA Portal) V11 project, we have included an empty STEP 7 (TIA Portal) V11 project for downloading in this FAQ response.

Download
The download contains the "compatibility_mode_V11_V12.zip" project.
Copy the "compatibility_mode_V11_V12.zip" file into a separate directory and then start the file with a double-click. You can then use STEP 7 to open and process the extracted project data.

compatibility_mode_V11_V12.zip ( 376 KB )

Note
More information is available in Entry ID 82169157 if in TIA Portal V13 you have to load project data from a device that has been configured with TIA Portal V12.

Creation environment
The download in this FAQ response was created with STEP 7 (TIA Portal) V11 SP2 Update 5.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.