×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 66620556, Entry date: 12/11/2012
(0)
Rate

SITRANS LR560 - Installation (video)

  • Entry
  • Associated product(s)
Video content Product Manager Tim Little shows how easy it is to install the SITRANS LR560 transducer on a silo. Each step is simple. In particular if the transducer has to be carried onto the roof of the silo. This is the first radar tansducer with a frequency of 78 GHz specially designed for bulk materials. ...

Video content
Product Manager Tim Little shows how easy it is to install the SITRANS LR560 transducer on a silo. Each step is simple. In particular if the transducer has to be carried onto the roof of the silo. This is the first radar tansducer with a frequency of 78 GHz specially designed for bulk materials.



Additional Keywords
eLearning, Tutorial, Video instructions, Fill level measurement


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.