×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 66825585, Entry date: 02/07/2019
(21)
Rate

TIA Portal project „Ready_for_Use“ & function block library for SIWAREX WP231

  • Entry
  • Associated product(s)

 Registrierung notwendig  READY_FOR_USE_LEGAL_FOR_TRADE.zip (38,7 MB) 

This example project is prepared for legal-for-trade scales together with the display SecureDisplay. Please note that legal-for-trade faceplates must match the approval certificate. The example project contains the SIWAREX WP231 function block (multiinstance ability) for the S7-1200 Basic Controller.

The .zip-file includes the following components:

  • TIA Portal V13 SP1 and V14 project with SIWAREX WP231 – TP700 Comfort – S7-1214 PLC V2.2
  • TIA Portal V13 SP1 and V14 project with SIWAREX WP231 – TP700 Comfort – S7-1214 PLC V3
  • TIA Portal V13 SP1 V14, V15 und V15.1 project with SIWAREX WP231 – TP700 Comfort – S7-1214 PLC V4

ATTENTION:
It’s important to choose the right project/library relating to the CPU firmware version!

  

 Registrierung notwendig  ready_for_use_s7.zip (86,8 MB) 

The example project/library contains the SIWAREX WP231 function block (multiinstance ability) for the S7-1200 Basic Controller V2, V3 and V4.

The .zip-file includes the following components:

  • TIA Portal V13 SP1 and V14 project with SIWAREX WP231 – TP 700 Comfort - S7-1214 PLC V2.2

  • TIA Portal V13 SP1 and V14 project with SIWAREX WP231 – TP 700 Comfort - S7-1214 PLC V3

  • TIA Portal V13 SP1, V14, V15 und V15.1 project with SIWAREX WP231 – TP 700 Comfort - S7-1214 PLC V4

  • TIA Portal V13 SP1, V14, V15 und V15.1function block library for S7-1200 PLC V2.2, V3.0 and V4.0

  • TIA Portal V14 SP1, V15 und V15.1 project with SIWAREX WP231 - KTP 400 Basic - S7-1214 CPU V4

ATTENTION:
It’s important to choose the right project/library relating to the CPU firmware version!

 

 Registrierung notwendig  ready_for_use_modbus.zip (68,6 MB)

The .zip-file includes the following components:

  • TIA Portal V12 SP1, V13 SP1, V14, V15 und V15.1 project with SIWAREX WP231 and directly connected TP700 Comfort Panel (Modbus-TCP-connection)
  • TP700 Restore Image, for direct download to TP700 Comfort via memory card / USB flash drive without TIA Portal software 

ATTENTION:
If the Restore-Image is used, the IP-address of the WP231 needs to be 192.168.0.21 (factory default)!

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit