×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 66867834, Entry date: 12/17/2012
(0)
Rate

SITRANS F M - Qualification Certificate for MAG 8000 & MAG 8000 CT

  • Entry
  • Associated product(s)
We are pleased to inform you that a Qualification Certificate feature is released for the MAG 8000 (7ME6810) and MAG 8000 CT (7ME6820). The MAG 8000 Qualification Certificate is an enhancement of the SIMATIC PDM tool released in EDD 01.02.00.15 (previously known as 'Soft Verificator'). The tool ...
We are pleased to inform you that a Qualification Certificate feature is released for the MAG 8000 (7ME6810) and MAG 8000 CT (7ME6820).

The MAG 8000 Qualification Certificate is an enhancement of the SIMATIC PDM tool released in EDD 01.02.00.15 (previously known as "Soft Verificator"). The tool generates a status report with key parameters collected from MAG 8000 & MAG 8000 CT meters. By cross checking the status report with the reference values defined in the document "Qualification Certificate Reference Guideline", the status quality of the device can be evaluated. The signed report serves as the customer’s qualification certificate.
 
 
 
The following support tools are accessible on the MAG 8000 Product Online Support webpage.
 
Please note that
  • The Qualification Certificate can be created on both the Advanced and the Basic version of MAG 8000 and MAG 8000 CT. The Insulation value, however, is 0 on the report generated with the Basic version of MAG 8000 and MAG 8000 CT because the Insulation Test functionality is not available with these meters. Therefore the Insulation value inspection in this case is N/A.
  • The Qualification Certificate feature is protected by an access code (the access code will be released in the Qualification Certificate Webinar in January 2013). It is highly recommended for service specialists to participate in the webinar, and go through the two documents above before executing this feature.

System Environment for Qualification Certificate

SIMATIC PDM 6.0 or later version

Please refer to SIEMENS Industry Mall

IrDA infrared interface adapter with USB for data acquisition with 1.2m cable

FDK:087L4163

FIELD PG Industrial Notebook (optional)

Please refer to SIEMENS Industry Mall

   

 
Download Info as PDF (139 KB) ( 139 KB ) . 
Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.