×
Siemens Industry Online Support
Siemens AG
Тип сообщения: Пример использования ID сообщения: 66926225, Дата сообщения: 04.07.2014
(3)
Оценить

Configuring of Electronic Signatures in SIMATIC PCS 7

  • Сообщение
  • Относится к продукту(ам)
Task In many industries, especially the pharmaceutical and food sector, there are often situations requiring different critical operator actions which have to be authorized by means of an Electronic Signature. Such kinds of operator actions may include, for example: adjusting a setpoint value exe...

Task
In many industries, especially the pharmaceutical and food sector, there are often situations requiring different critical operator actions which have to be authorized by means of an Electronic Signature. Such kinds of operator actions may include, for example:

  • adjusting a setpoint value
  • executing a switching operation
  • starting a sequence of operations
  • starting a batch operation
Depending on the specific task, an operation may require a 4-eyes principle. This means that an operation must be approved by at least two different persons. Release shall be given with the help of an Electronic Signature which, for traceability purposes, shall be stored in a long-term archive. The archive entries must be suitable to identify which operations have been performed by whom and when, including the date and time of their acknowledgement.

Solution
In order to perform critical operator actions at the PCS 7 operator systems, this intervention must be verified by one or more users with an Electronic Signature. Authentication of the individual users is effected with SIMATIC Logon by means of an authorization prompt. The persons with Electronic Signature authorization are defined in the different user groups. When all required signatures are available, the critical operation will be executed. The associated signature data (time, user, operator action, operator station) will be written to the PCS message archive in the form of an audit trail.

Your Benefits at a Glance

  • dialog-based configuration of multiple, role-based Electronic Signatures
  • easy integration of the “Electronic Signature” functions in a PCS 7 project
  • reduced costs and minimized configuration time through the use of preconfigured modules
  • the plant is operated only by authorized personnel, thus increasing the protection against faults and errors
  • excellent traceability of significant operator actions
  • easy documentation by means of automatically generated audit trails in PCS 7
  • long-term archiving of the Electronic Signatures ensured by the PCS 7 archiving concept

This application example supports you in engineerinig of electronic signature functions. The downloadable ZIP archive contains the installation files. With the installation all necessary files and scripts as well as a demo project are copied onto your computer. In the documentation you will find the description to the demo project as well as step-by-step instructions for configuring of electronic signatures.

Validity
The instructions and the demo project were created with SIMATIC PCS 7 V8.0 SP1 and SIMATIC Logon V1.5.

Downloads
  Configuring of Electronic Signatures in SIMATIC PCS 7 (1,9 MB)
 Registrierung notwendig  Setup of the functions and modules (265,7 MB)

Указания по безопасности
Для обеспечения и дальнейшего поддержания кибер-безопасности технической инфраструктуры, систем, машин и сетей необходимо внедрить комплексную концепцию информационной безопасности, которая соответствует последним достижениям науки и техники. Продукты и решения Сименс являются всего лишь одним из компонентов такой концепции. Более подробную информацию о кибер-безопасности можно получить здесь
https://www.siemens.com/cybersecurity#Ouraspiration.
Оценить сообщение
без оценки
Вопросы и обратная связь
Что вы хотите сделать?
Примечание: отзыв всегда относится к текущей статье / текущему продукту. Ваше сообщение будет перенаправлено техническим редакторам службы онлайн-поддержки. В течение нескольких дней вы получите ответ, если ваш отзыв содержит вопрос. Если у нас не возникнут вопросы по вашему отзыву, мы не будем вас беспокоить.
Поддержка статистики
Данная функция позволяет выдавать идентификаторы (ID) результата поиска согласно желаемому количеству (формат .txt)

Генерировать список
Копировать URL
Отобразить эту страницу в новом дизайне
Панель управления mySupport
Тематические страницы для данных записей