×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 67121011, Entry date: 02/14/2019
(12)
Rate

PC-based Automation: Simple Migration of S7-300/S7-400 - projects to S7-1500 Software Controller with TIA Portal (STEP 7 and WinCC)

  • Entry
  • Associated product(s)
You want to change an existing automation solution with S7-300/S7-400 and HMI panel to Open Controller (S7-1500 Software Controller und WinCC Runtime Advanced).

This application example shows how to migrate a project with S7-300 to a S7-1500 Software Controller and how to migrate a Comfort Panel to SIMATIC WinCC RT Advanced.

The figure below provides an overview of the automation task and which hardware (gray box) should be migrated. The remaining hardware will be migrated without changes.


Fig. 1

Migration to Open Controller (S7-1500 Software Controller and WinCC RT Advanced)
The following figure gives a schematic overview of the most important components of the solution and the components after migration (gray box).
 


Fig. 2


The example shows you how...

  • the program will be migrated from CPU 315-2 PN/DP to S7-1500 Software Controller.
  • the connections between Database PC, ET 200SP station and SINAMICS G120 will be made to S7-1500 Software Controller.
  • the visualization of TP1200 Comfort will be migrated to WinCC RT Advanced.

Downloads
  Documentation (1,5 MB) 
 Registrierung notwendig  Project (TIA Portal V15.1) (81,4 MB) 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.