×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 67385235, Entry date: 11/02/2017
(4)
Rate

SINAMICS G120 firmware version 4.6 HF22

  • Entry
  • Associated product(s)
In this article you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.6 HF22.

Important Note

The SINAMICS G120 Firmware Version 4.6 has achieved the milestone P.M410 "Product Cancellation" on 01.10.2017. With this background, we recommend using the latest SINAMICS G firmware.


Details concerning this Milestone, please refer to the following article 109751467.


Content of the SINAMICS G120 multicard

In this article you will find the download as well as the ordering information for SINAMICS G120 multicard with version V4.6 HF22.

 

The version designation on the multicard is SINAMICS G120 V04.06.00.22. The internal firmware version number is SINAMICS G120 V04.60.21.48.

The SINAMICS G120 multicard contains the firmware releases for the following G120 products: 
 

 SINAMICS Family
Product 
Firmware (FW) Version 
Internal FW version ID
G120PCU230P-2V4.6 HF22V04.60.21.48
G120

CU240B-2

CU240E-2

CU250S-2

V4.6 HF22V04.60.21.48
G120CG120C V4.6 HF22V04.60.21.48
G120DCU240D-2
CU250D-2 
V4.6 HF22V04.60.21.48

 

When upgrading, please follow the instructions for Firmware update.

 

Note:
Only Control Units CU240B-2, CU240E-2, CU240D-2, CU250D-2 and G120C from firmware release V4.5 can be upgraded to the SINAMICS G120 firmware version 4.6.


Third-party software - Licensing terms and copyright information

You can find the copyright information for third-party software contained in this product, particularly open source software, as well as applicable licensing terms of such third-party software in the READ_OSS.HTM file.


Special information for resellers 
The information and the license terms in the READ_OSS.HTM file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.


Availability of Source Code
Certain license conditions of third-party software components used in this product may require Siemens to provide you with the source code and additional information for such components. In most cases, Siemens provides this information on or with the device. In case Siemens is technically unable to do so, you may request a copy of of this OSS source code against payment of shipping and handling charges. Please send your request to the address provided at the end of this section.



Siemens AG 

Digital Factory

Customer Services DF&PD

DF CS SD CCC TS

Gleiwitzer Str. 555

90475 Nuernberg, Deutschland

Internet: http://www.siemens.com/automation/support-request

Tel.: +49 911 895 7222


  READ_OSS.HTM (1,3 MB)


Actual list of secondary conditions for the SINAMICS G120, firmware V4.6

   sinamics_g120_v4_6_restrictions.pdf (38,9 KB)

  

Corrected functional restrictions for SINAMICS G120, firmware V4.6 HF22
  Corrected_functional_restrictions_G120_V4_6_HF22.pdf (35,0 KB)

 

Instructions for updating the firmware of the SINAMICS G120

When upgrading, please refer to the instructions, Chapter "Firmware update" in the operating instructions of the particular Control Unit.

 

For example, the instructions for the firmware update for the CU240B-2 and CU240E-2 can be found here:

 

  instructions_firmwareupdate_g120_cu240be-2_eng.pdf (411,2 KB)

 

Note:

The zip file must be saved unpacked on the SD card in the root directory.

An SD memory card with at least 256 MB must be used.

Memory cards larger than 2 GB are not supported.

 

Provision of the SINAMICS G120 multicard

The content of the SINAMICS G120 multicard described above can be downloaded here:

  • Content of the SINAMICS G120 multicard V4.6 HF22:
     Download unterliegt Exportcontrolle  SINAMICS_G120_firmware_V4_6_HF22.zip (242,5 MB)

    Note:
    The software is subject to export restrictions.
    The download is only available to registered users.

    Due to export regulations a download is only possible within the EU.

 

Alternatively, the SINAMICS G120 multicard V4.6 (SD card) can be ordered using the following order number 6SL3054-7EG00-2BA0 .

 

List of faults and alarms

List of faults and alarms for CU230P-2

The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120P in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120P product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu230p_v04601800_chs.xml (339,8 KB)
  alarmlist_g120_cu230p_v04601800_eng.xml (363,7 KB)
  alarmlist_g120_cu230p_v04601800_esp.xml (377,0 KB)
  alarmlist_g120_cu230p_v04601800_fra.xml (384,9 KB)
  alarmlist_g120_cu230p_v04601800_ita.xml (381,4 KB)
  alarmlist_g120_cu230p_v04602000_deu.xml (369,6 KB)

 

List of faults and alarms for the CU240B-2 and CU240E-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu240b_e_v04601800_chs.xml (541,0 KB)
  alarmlist_g120_cu240b_e_v04601800_eng.xml (578,5 KB)
  alarmlist_g120_cu240b_e_v04601800_esp.xml (608,0 KB)
  alarmlist_g120_cu240b_e_v04601800_fra.xml (623,0 KB)
  alarmlist_g120_cu240b_e_v04601800_ita.xml (611,3 KB)
  alarmlist_g120_cu240b_e_v04602000_deu.xml (589,4 KB)

 

List of faults and alarms for the CU240D-2 and CU250D-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120D in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120D product is concerned, no additional support can be guaranteed here.

  alarmlist_g120d_v04601800_chs.xml (632,5 KB)
  alarmlist_g120d_v04601800_eng.xml (677,4 KB)
  alarmlist_g120d_v04601800_esp.xml (705,5 KB)
  alarmlist_g120d_v04601800_fra.xml (722,9 KB)
  alarmlist_g120d_v04601800_ita.xml (710,7 KB)
  alarmlist_g120d_v04602000_deu.xml (686,7 KB)

 

List of faults and alarms for CU250S-2
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120 in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120 product is concerned, no additional support can be guaranteed here.

  alarmlist_g120_cu250s_do_v04601800_chs.xml (1,7 MB)
  alarmlist_g120_cu250s_do_v04601800_eng.xml (1,8 MB)
  alarmlist_g120_cu250s_do_v04601800_esp.xml (1,9 MB)
  alarmlist_g120_cu250s_do_v04601800_fra.xml (2,0 MB)
  alarmlist_g120_cu250s_do_v04601800_ita.xml (1,9 MB)
  alarmlist_g120_cu250s_do_v04602000_deu.xml (1,9 MB)

 

List of faults and alarms of the G120C
The "alarmlist_*.xml" files are not necessary for the correct operation of the firmware and the associated STARTER. They only include an export of the "Alarm messages" text for the G120C in the "xml" format.
Customers occasionally request these exported texts so that they can further process them in their own applications or integrate them in external devices. As a consequence, as far as the G120C product is concerned, no additional support can be guaranteed here.

  alarmlist_g120c_v04601800_chs.xml (358,8 KB)
  alarmlist_g120c_v04601800_eng.xml (386,2 KB)
  alarmlist_g120c_v04601800_esp.xml (406,5 KB)
  alarmlist_g120c_v04601800_fra.xml (415,9 KB)
  alarmlist_g120c_v04601800_ita.xml (408,9 KB)
  alarmlist_g120c_v04602000_deu.xml (393,2 KB)

 

GSD files for project integration into the PROFIBUS configuring tool

PROFIBUS GSD files can be downloaded in the following entries:

GSDML files for project integration into the PROFINET configuring tool

PROFINET GSDML files are can be downloaded in the following entries:

 

EDS files for project integration into the CANopen configuring tool

The EDS files for project integration in the CANopen configuring tools can be downloaded from the following entry:  (see 48351511)

 

STARTER

STARTER Version 4.3 SP2 and higher is required to use the new functions of this firmware version V4.6. (see 64374921)

 

IOP

Note

If the SINAMICS G120P (CU230P-2), G120 (CU240B-2, CU240E-2, CU250S-2), G120D (CU240D-2, CU250D-2) and G120C products are operated with firmware version 4.6 and an Intelligent Operator Panel (IOP) is used, then for this purpose, the IOP firmware from version V1.4 should be used. (see 73159342)

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.