×
Siemens Industry Online Support
Siemens AG
Entry type: Application example, Entry ID: 67460624, Entry date: 07/25/2017
(44)
Rate

PRONETA 2.4.0.44 Commissioning and Diagnostics Tool for PROFINET

  • Entry
  • Associated product(s)
PRONETA is a free tool for the analysis and configuration of PROFINET networks with special support for ET 200 distributed IO. The IO Test can provide support with the quick and comfortable examination and documentation of a plant's wiring.



Fig. 01
 
SIEMENS PRONETA is a free PC-based software tool which provides assistance with regard to  the diagnostics and commissioning of PROFINET networks in automation systems by providing the following features:
  • Topology overview, which automatically scans your PROFINET and displays all connected devices. The list of all connected devices can be exported, including the details of all electronic modules. PRONETA allows for configuring components, and other simple configuration tasks, as well as for a comparision between the actual installation and a reference plant.
  • IO Test for the rapid test of the wiring and module configuration of the components. By reading and writing inputs and outputs, PRONETA ensures that the connections between distributed IO components and their sensors and actuators have been set up properly. PRONETA can create test profile templates and save test protocols to document test results.
  • All tasks can be accomplished even before a CPU has been linked up with the network. Since no further engineering tools besides PRONETA and no dedicated hardware are required, PRONETA facilitates a quick and comfortable check of a plant configuration at an early stage.

New features of SIEMENS PRONETA V2.4

  • Improved user interface with German language support
  • Topology comparison with additional options
  • I/O test supports SIRIUS motor starters and SIPLUS heating control units HCS4200/4300
  • Extended report functionality

Requirements

  • Hardware
    SIEMENS PRONETA runs on any standard PC, PG or Laptop. The PROFINET connection is established through a regular Industrial Ethernet cable.
  • Software
    PRONETA is released for Windows 7, Windows 8 and Windows 10 (each with 32 or 64 Bit).
    In addition to PRONETA, the .NET Framework v4.6.1 must be installed on the PC.

Installation
To start and install the software tool, proceed according to the documentation.

Downloads

 Registrierung notwendig  PRONETA 2.4 (18,2 MB)
SHA256 checksum: 3A4F79269700F1EBC661A8216479F07981A60C88F58F145442356A3356E3EBCB

Videos

Further Information
PRONETA Website

Support
If you have any questions regarding SIEMENS PRONETA please contact us at
proneta.industry@siemens.com.

Last change
adapted to software version 2.4


Additional Keywords
io-check diagnosis analysis

Security information
In order to protect plants, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art industrial security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about industrial security, please visit
http://www.siemens.com/industrialsecurity.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
mySupport Cockpit