×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 67460624, Entry date: 06/23/2021
(93)
Rate

PRONETA Basic 3.2 Commissioning and Diagnostics Tool for PROFINET

  • Entry
  • Associated product(s)
The PROFINET network analyzer PRONETA Basic is a simple tool intended for the rapid analysis and configuration of PROFINET networks and the simple testing of ET 200 distributed IO systems and other components.





PRONETA Basic is well suited for solving two tasks fundamental to the commissioning of PROFINET installations:

  • The “Network Analysis" task gives a quick overview of the devices connected to PROFINET. It features simple configuration options, like setting network parameters or assigning a network name to the devices which are part of the subnet the PRONETA PC is connected. The application also provides powerful mechanisms to compare several network topologies with each other, for example to compare an “ideal” topology intended for a project with the actual installation.
  • The “IO Test" task is a simple and intuitive method to test the IO wiring of an installation with numerous distributed IO devices. It allows for checks of the wiring and will automatically set up a protocol of the test procedure which can be exported for documentation purposes.
Both tasks can be performed before a CPU is integrated in the network. Since there are no other engineering tools required, PRONETA Basic allows fast and convenient checks of the system configuration from early on.

New features of PRONETA Basic V3.2

  • Support for the IO test of central IO modules of most SIMATIC S7-1500 CPUs and ET 200SP CPUs.**)
  • Read out diagnostic information for all devices
  • Include devices found via IP forwarding in other subnets
  • Various bugfixes and performance improvements

**)  Fail-safe central IO modules are not supported.

PRONETA Professional
Beside the free PRONETA Basic, there is now also the licensed product PRONETA Professional, which extends the PRONETA Basic functionality by providing an API, based on MQTT communication, which allows the automated and remotely conducted scan of PROFINET networks.
PRONETA Professional in the SIEMENS Mall

PRONETA Requirements

  • Hardware
    PRONETA Basic runs on any standard PC, PG or laptop. The PROFINET connection is established through a regular Industrial Ethernet cable.
  • Software
    PRONETA Basic is released for Windows 7, Windows 7 Embedded Compact, Windows 8 and Windows 10 (each with 32 or 64 bits).
    In addition to PRONETA Basic, the .NET Framework v4.6.2 must be present on the PC.

Starting
 To start the software tool, proceed according to the documentation.

Downloads

 Registrierung notwendig  proneta_3_2_0_0.Zip (287,2 MB)(SHA-256)405f374044d25f789f254cb048e2c49e18de7baddc62ba9235b50207193f903e

 Registrierung notwendig  List of supported modules (28,3 KB)


SHA256-Prüfsumme: 9BFC2E7AF19C00C72F1426B057C638BFDA4CE7020F398B6F100DFB4F716E74AA
(Source code for OSS components used by PRONETA, download is not mandatory)
   
Videos

Further Information
PRONETA Website

Support
If you have any questions or problems regarding the application of PRONETA, please contact
proneta.industry@siemens.com 


Last Changes
Update to software version 3.2

Additional Keywords
io-check

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit