×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 67460624, Entry date: 06/28/2019
(59)
Rate

PRONETA 2.7.0.3 Commissioning and Diagnostics Tool for PROFINET

  • Entry
  • Associated product(s)
PRONETA is a free tool for the analysis and configuration of PROFINET networks with special support for ET 200 distributed IO. The IO Test can provide support with the quick and comfortable examination and documentation of a plant's wiring.



Fig. 01
 

SIEMENS PRONETA is a free PC-based software tool which provides assistance with regard to the commissioning of PROFINET plants by providing the following features:

  • Topology overview, which automatically scans your PROFINET and displays all connected devices. This overview can be exported in the form of a device list. There is the option to name the components and to perform other basic configuration tasks and also to compare a reference system with the actually installed configuration.
  • IO Test for the rapid test of the wiring and module configuration of the components. By reading and writing inputs and outputs, PRONETA ensures that the connections between distributed IO components and their sensors and actuators have been wired properly. PRONETA can create test profile templates and save test protocols to document test results.
  • All tasks can be accomplished even before a CPU has been linked up with the network. Since no further engineering tools besides PRONETA and no dedicated hardware are required, PRONETA facilitates a quick and comfortable check of a plant configuration at an early stage.

New features of SIEMENS PRONETA V2.7

  • Various bugfixes and performance improvements

PROFINET Professional
Beside the free PRONETA, there is now also the licensed product PRONETA Professional, which extends the PRONETA functionality by providing an API, based on MQTT communication, which allows the automated and remotely conducted scan of PROFINET networks.
PRONETA Professionalin the SIEMENS Mall

PRONETA Requirements

  • Hardware
    SIEMENS PRONETA runs on any standard PC, PG or laptop. The PROFINET connection is established through a regular Industrial Ethernet cable.
  • Software
    PRONETA is released for Windows 7, Windows 7 Embedded Compact, Windows 8 and Windows 10 (each with 32 or 64 bits).
    In addition to PRONETA, the .NET Framework v4.6.1 must be installed on the PC.

Installation
To start and install the software tool, proceed according to the documentation.

Downloads

SHA256 checksum: 404DC660F962B5E4A67BF3BED7FE1AD8F452A8F63B10131C4D817D32D41A97A4


SHA256-Prüfsumme: C590E0BB8450DA9795F3897DDF6A907687441CF456554C0FE2BC5554B6E3CD36
(Source code for OSS components used by PRONETA, download is not mandatory)
   
Videos

Further Information
PRONETA Website

Support
If you have any questions or problems regarding the application of SIEMENS PRONETA, please contact
proneta.industry@siemens.com 

Last Changes
Update to software version 2.7

Additional Keywords
io-check

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit