×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 68011497, Entry date: 09/15/2020
(12)
Rate

System Diagnostics with S7-1500 and TIA Portal

  • Entry
  • Associated product(s)
When a system error occurs, hardware components and devices of other manufacturers can trigger a system reaction. The hardware components provide information on the system error that has occurred. For S7-1500 PLCs, the system diagnostics provides a convenient way to evaluate this diagnostic information and display it in the form of alarms.
Task
In the automation technology, diagnostics of devices, modules and networks are gaining importance. Diagnostics over the whole system can minimize downtimes. The automation task consists of monitoring a PROFINET IO peripheral system with various network components. The possibility of an individual diagnosis of the components and a detailed diagnosis of the complete system should be guaranteed. The priority is on the collection and display of the diagnostic information.

The figure below provides an overview of the automation task.

Solution
The system diagnostics are integrated in the firmware of the CPU S7-1500 and work independently from cyclic user programs. Therefore it is also available in the CPU operating mode STOP. Any faults are detected immediately and reported to the higher-level HMI device, the web server, the display of the CPU S7-1500, the LED displays in the module concerned and in the TIA Portal even in the operating mode STOP. Therefore, the system diagnostics are always synchronous with the actual system status.

This application describes:

  • the various display possibilities of the System Diagnostics
  • how you can configure the System Diagnostics quickly and easily, using a few examples
  • the System Diagnostics with the user program.

The following picture shows the most important components of the solution with an S7-1500.

  1. The device detects a fault and sends diagnostic data to the assigned CPU.
  2. The CPU informs the connected display media. The display of the system diagnostics is refreshed.

Advantages

  • Integrated System Diagnostics
    The integrated System Diagnostics ensure full transparency of the system status. The system diagnostics are generated automatically.
  • Uniform display concept
    The system diagnostics information is displayed as a uniform clear text information in the CPU display, TIA Portal, HMI and the web server itself for messages of the drives.
  • Channel granular display concept
    In case of failure, the respective channel can be detected and classified quickly.

Benefit

  • Reduced downtimes and increased system availability thanks to an exact visual allocation in case of failures.
  • Efficient failure analysis due to a uniform display concept.
  • Servicing possible without a current project, due to a complete project upload including symbols.


Documentation and Project
 
  Documentation (3,0 MB)
 Registrierung notwendig  STEP 7 Project (V16 Update 1) (9,8 MB)


Further Information
 
Application example - Diagnostics in User Program with S7-1500


Last change
Update to TIA Portal V16 Update 1

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.