×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 68011827, Entry date: 05/13/2019
(2)
Rate

3-Point Stepper Control with SIMATIC S7-1500

  • Entry
  • Associated product(s)
STEP 7 (TIA Portal) offers you the technology object "PID_3Step" to control valves and actuators with integrating behavior for SIMATIC S7-1200/S7-1500 PLC.

Description
The technology object "PID_3Step" controls the valve of a mixer tap according to a desired given temperature.
A three-way mixing valve with valve actuator is used. The valve is digital controlled in both directions. This is referred to as a 3-point stepper control.
Varying the valve position can yield any mixing ratio of hot and cold entering water and so the water outlet temperature.


Figure 01

Note
This entry won't be updated anymore because this application example is published together with the version for SIMATIC S7-1200 under the following link: Application Example "3-Point Stepper Control with SIMATIC S7-1200/S7-1500"