Entry type: Application example Entry ID: 68014632, Entry date: 08/09/2017
(41)
Rate

Creating Faceplates with WinCC Runtime Advanced and Comfort Panels

  • Entry
  • Associated product(s)
Useful information on the topic of “HMI faceplates” and how to use HMI faceplates as a user.

In serial machine construction, functions such as drive on/off, switchover automatic/manual mode etc. are frequently used. These functions generally only need to be adjusted to the respective machine and its control tags. Using preprogrammed objects reduces engineering times and costs.

Solution
Learn the basics for creating faceplates and use their advantages for their configuration. Using this document helps you generate your own faceplates independently. The application gives several examples with step-by-step instructions for creating a faceplate.
The created examples are stored in the enclosed HMI configuration.
 


Advantages
This application example on hand offers you the following advantages:

  • The basics, functions and properties of faceplates are described.
  • The step-by-step instruction for creating a faceplate and the practical application examples reduce the familiarization time.
  • Faceplates increase the efficiency.
    Storing the faceplate in a library enables calling and using them easily in different projects.
  • Avoiding errors through a simple connection to the STEP 7 control program.

Documentation and example project
 Getting Started for HMI faceplates (636,9 KB)
  Basics on HMI faceplates (2,8 MB)
 Application examples for HMI faceplates (2,4 MB)
 Example project (9,2 MB)

Trainings for WinCC (TIA Portal) and Panels near you
SITRAIN basic training: 109758624
SITRAIN advanced training: 109758626 

Further Information
Sample Blocks for WinCC (TIA Portal) and STEP 7 (TIA Portal) (for S7-1200 and S7-1500 in SCL)
Faceplates for the Visualization of Sentron PAC Power Meters for WinCC Runtime Professional
Sample Blocks for WinCC V7 and STEP 7 (TIA Portal) (for S7-1200 and S7-1500 in SCL)
Machine-oriented operator control and monitoring in Online Support

Last Changes
Update to TIA Portal V14

Additional Keywords
Structure, panel, panels, faceplates, picture objects, grouping elements

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.