×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 68015276, Entry date: 03/20/2013
(42)
Rate

Service Pack 3 for STEP 7 V5.5 and STEP 7 Professional 2010

  • Entry
  • Associated product(s)
Service Pack 3 for STEP 7 V5.5 and STEP 7 Professional 2010

DESCRIPTION:

Download  of Service Pack 3 for STEP 7 V5.5

Installation requirements:

  • STEP 7 V5.5 (with or without Service Pack) 
  • STEP 7 Professional 2010 (with or without Service Release)

i.e. to be able to install Service Pack 3, STEP7 V5.5 or STEP 7 Professional 2010 must already be installed on your computer.

Please also read the information (What’s NEW, special hints, etc.) which we have compiled for you in entry ID67878325.

Customers with a valid Software Update Service agreement for STEP 7 will receive the DVD with STEP 7 V5.5 incl. SP3 automatically.

Customers with a valid Software Update Service agreement for STEP 7 Professional will receive the DVD with the STEP 7 Professional Edition 2010 Service Release 3 automatically. The SP3 for STEP 7 V5.5 is part of this DVD (see entry ID 67878325 ).

If you wish to change to a new operating system, please bear the following in mind:

  • It is not permitted/possible to change to another operating system if STEP 7 is installed already. Before you change the operating system, please be sure to uninstall STEP 7 and any other possibly installed STEP 7 option packages.
  • Before you change the operating system the existing authorization / License Key must be saved to a floppy disk or USB stick with the program AuthorsW / Automation License Manager.
  • If you wish to change to MS Windows 7 64-Bit with STEP 7, you require the DVD of STEP 7 V5.5 Service Pack 1 and higher.
  • If you wish to change to MS Windows 7 64-Bit with STEP 7 Professional, you require the DVD of STEP 7 Professional Edition 2010 Service Release 1 and higher.

Customers without Software Update Service agreement can obtain the SP3 as follows:

  1. Order a DVD:  You can order the Trial License with STEP 7 V5.5 incl. Service Pack 3 on DVD.
    The order no. is: 6ES7810-4CC10-0YA7

    For the current STEP 7 Professional you can obtain a Trial License with the STEP 7 Professional Edition 2010 SR3.
    The DVD with the STEP 7 Professional Edition 2010 Service Release 3 also includes the SP3 of STEP 7 V5.5
    The order no. is: 6ES7810-5CC11-0YA7

  2. Free Download
    As usual, we are offering a free download:


    Service Pack 3 for STEP 7 V5.5

     Registrierung notwendig  simatic_step7_v55_sp3.zip (1,3 GB)

    This free download includes the SP3 for STEP 7 V5.5 and NCM.


 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.