×
Siemens Industry Online Support
Siemens AG
文档类型 软件下载 文档编号 68034568, 文档发布日期 2019年4月26日
(196)
评估

SINAMICS Startdrive V14 SP1

  • 文档
  • 涉及产品
You can find the current Startdrive version here.

SINAMICS Startdrive V14 SP1 can also be ordered directly as a DVD (6SL3072-4EA02-0XA0).

OSS note regarding SINAMICS Startdrive V14 SP1

Third-party software – license conditions and copyright notes
You can find the copyright notes on the third-party software, especially Open Source Software, as well as applicable license conditions for this type of third-party software in the following file:

 Registrierung notwendig  Readme_OSS_All_Languages.htm (1.5 MB)

Special note for resellers
The information and the license conditions in the ReadMe_OSS.htm file must be passed on to the purchasing party to avoid license infringements by the reseller or purchasing party.

OSS source code
The OSS source code files are part of the download package and can be downloaded separately here:

 Registrierung notwendig  OpenSourceSoftware_SDR_G120_V14SP1.zip (723.3 KB) 

Note:
There is only one download package for Startdrive V14 SP1. It is not split up into two separate packages, "Option package for STEP 7" and "Startdrive Standalone". Startdrive V14 SP1 supports both installation variants.

You can find the Startdrive commissioning tool for the SINAMICS G120 drive family here.

SINAMICS Startdrive V14 SP1 

SINAMICS Startdrive V14 SP1

Associated sales information under 109746259 

 Registrierung notwendig  Startdrive_V14_SP1.zip (2.3 GB)

SHA-256 checksum:

D02AB766C818440053C8F21FCD6CE5C5DEEF85355325574BF1492B120B44D50D

SINAMICS Startdrive V14 SP1 Update 1

Associated sales information under 109746504 

 Registrierung notwendig  Startdrive_V14_SP1_Update_1.zip (1.5 GB)

SHA-256 checksum:

D6802DA47AA4C41C7E10CCF6DEA71D627545FDA77885557CA23E7F285321BE0C

SINAMICS Startdrive V14 SP1 Update 3

Associated sales information under 109747521 

Update 3 has been withdrawn.

SINAMICS Startdrive V14 SP1 Update 4

Associated sales information under 109749513 

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_4.001 (1.5 GB)

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_4.exe (2.8 MB)

SHA-256 checksum:  Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_4.txt (1 KB) 

Information on the SHA-256 checksum 109483101

SINAMICS Startdrive V14 SP1 Update 5

Associated sales information under 109752536

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_5.001 (1.5 GB)

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_5.exe (2.8 MB)

SHA-256 checksum:  Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_Update_5.txt (1 KB)

Information on the SHA-256 checksum 109483101

SINAMICS Startdrive V14 SP1 Update 6

Associated sales information under 109755213

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD6.exe (1.6 GB) 

SHA-256 checksum  Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD6.txt (1 KB)

Information on the SHA-256 checksum 109483101

SINAMICS Startdrive V14 SP1 Update 7

Associated sales information under 109758855 

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD7.exe (1.6 GB)

SHA-256 checksum  Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD7.txt (1 KB) 

Information on the SHA-256 checksum 109483101 

SINAMICS Startdrive V14 SP1 Update 8

Associated sales information under 109768196 

 Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD8.exe (1.6 GB)

SHA-256 checksum  Registrierung notwendig  SINAMICS_Startdrive_V14_SP1_UPD8.txt (1 KB) 

Information on the SHA-256 checksum 109483101 

SINAMICS Startdrive can be used free of charge without entering a license key.

Startdrive supports Chinese (simplified), English, French, German, Italian and Spanish.

Installation procedure for Startdrive V14 SP1

  1. Download the attached ZIP file.
  2. Unpack the ZIP file into a target directory on your hard disk. Please ensure that there are no spaces in the entire path name of this target directory.
  3. Launch Startdrive by calling up Start.exe.


 Startdrive V14 SP1 Support Package for SINAMICS firmware V4.7 SP9

Startdrive V14 SP1 Support Package for SINAMICS firmware V4.7 SP9

Associated sales information under 109751653 

 Registrierung notwendig  Startdrive_V14SP1_HSP_FW_V4_7_SP9.zip (451.5 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_V14SP1_HSP_FW_V4_7_SP9.txt (1 KB) 

Information on the SHA-256 checksum 109483101

Note:
Startdrive V14 SP1 Update 5 is a requirement for the installation of the Support Package for SINAMICS firmware V4.7 SP9.



 Startdrive V14 SP1 Support Package for SINAMICS firmware V4.7 SP10

Startdrive V14 SP1 Support Package for SINAMICS firmware V4.7 SP10

Associated sales information under 109765695 

 Registrierung notwendig  Startdrive_V14SP1_HSP_FW_V4_7_SP10.zip (463.6 MB)

SHA-256 checksum  Registrierung notwendig  Startdrive_V14SP1_HSP_FW_V4_7_SP10.txt (1 KB) 

Information on the SHA-256 checksum 109483101 

Restricted compatibility when using the Support Package:
Please note that the compatibility with other Startdrive versions may be restricted when using the Support Package. Please observe the information provided at: 109765544 

Note:
Startdrive V14 SP1 Update 7 is a requirement for the installation of the Support Package for SINAMICS firmware V4.7 SP10: 109758855

Installation notes for Startdrive V14 SP1 Support Packages

At 54163658 you will find a description of the procedure for updating the hardware catalog of your Startdrive (TIA Portal) installation with this download.

The Support Packages can only be installed if Startdrive V14 SP1 has already been installed. If Startdrive V14 SP1 is installed again, the corresponding Support Package must also be installed again.


Download of previous versions


Notes about downloading

As a result of security settings, the download may be classified as a security risk, as shown in the screenshot. In order to avoid problems after installation, ZIP files must be classified as harmless after downloading by
right clicking on > Properties > "Allow" button.


Additional search terms

FB284, FB285, FB286, blocks, SINA_POS, SINA_SPEED, SINA_PARA

安全性信息
为了保护技术基础设施、系统、机器和网络免受网络威胁,有必要实施并持续维护一个全面、最先进的IT安全方案。西门子的产品和解决方案构成了这一方案的一个要素。有关网络安全的更多信息,请访问
https://www.siemens.com/cybersecurity#Ouraspiration.
评估文档
无评估
请求和反馈
您想要做什么?
注意:反馈总是与当前的条目/产品相关。您的消息将被转发给我们在线支持团队的技术编辑们。如果我们需要就您的反馈提供答复,您将在几天内收到答复。如果没有其它问题,您将不会收到答复。