×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 68057757, Entry date: 08/28/2015
(0)
Rate

Where can you find the technical data sheets and safety data sheets of the backup batteries for the SIMATIC S5 and Simadyn?

  • Entry
  • Associated product(s)

The following backup batteries can be used for the SIMATIC S5 as well as Simadyn.

  • SL-360: Article number 6ES5980-0AE11
  • SL-350: Article number 6ES5980-0MA11
  • SL-2770: Article number 6EW1000-7AA

The above-mentioned backup batteries are LTC batteries (Lithium thionyl chloride) made by TADIRAN.

At the link below you can download the technical data sheets and safety data sheets of the above-mentioned TADIRAN LTC batteries.

TADIRAN BATTERIES

Further Information
Entry7379933 provides information about which backup batteries can be used for the SIMATIC S5.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.