×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 68170195, Entry date: 03/29/2018
(0)
Rate

Firmware Updates for FF LINK, IM 153-2 FF OUTDOOR

  • Entry
  • Associated product(s)
A collection of firmware updates is availale for FF LINK, IM 153-2 FF OUTDOOR

When updating the operating system, you should always update to the latest version available for the product with the relevant order number. The previous versions of the operating system are intended only as a backup, permitting you to downgrade again to the original version, which however has not been necessary in any known case as yet. The latest version of an FF-Link firmware is valid for all the releases of that order number.

What's new?

  • Improved behaviour in collaboration with SIMATIC PDM >= V8.2 (V1.0.3)

Online firmware update with STEP7 HW-Config

  1. Download the required firmware file
  2. Unpack the file by double-clicking the file name
  3. Select the corresponding FF-Link in HW-Config  
  4. Program the firmware by selecting: "Target System/ Update Firmware" in the program menu
  5. Earmark the directory with the firmware file in the dialog box and start the firmware download

The download process is not visible on the FF-Link. After the download is completed the new firmware can be started automatically, or by means of power OFF/ON.

Online firmware update with SIMATIC Manager

  1. Download the required firmware file
  2. Unpack the file by double-clicking the file name
  3. Connect the programming device to the line to which the FF-Link is connected
  4. Open the view "Accessible Nodes" in the Simatic Manager and select the station address
  5. Program the firmware by selecting: "Target System/PROFIBUS/Update Firmware" in the program menu
  6. Earmark the directory with the firmware file in the dialog box and start the firmware download.

The download process is not visible on the FF-Link. After the download is completed the new firmware can be started automatically, or by means of power OFF/ON

Overview of order numbers and latest versions of the FF-Link, IM 153-2 FF OUTDOOR

Order Number

Firmware Version

Upgrade with ...
6ES7 153-2DA80-0XB0V1.0.3Recommended for upgrade
 Download unterliegt Exportcontrolle 1532DA80 V1.0.3 (508,0 KB) 
 Registrierung notwendig SHA-256 checksum(1 KB) 

V1.0.2

Backup only
 Download unterliegt Exportcontrolle 1532DA80 V1.0.2 (487,6 KB) 
 Registrierung notwendig  SHA-256 checksum (1 KB) 

V1.0.1

Backup only
 Download unterliegt Exportcontrolle 1532DA80 V1.0.3 (487,4 KB)
 Registrierung notwendig SHA-256 checksum(1 KB) 
 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.