×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 68202648, Entry date: 05/22/2013
(1)
Rate

Delivery release for SIMOTION Version V4.3 SP1 HF12

  • Entry
  • Associated product(s)

With immediate effect, the SIMOTION Version V4.3 SP1 HF12 has been released for delivery.

The release includes the SIMOTION SCOUT Engineering System and SCOUT Stand-alone V4.3 SP1 HF12 as well as the SIMOTION Runtime Software V4.3 SP1 HF12, which is supplied with the SIMOTION SCOUT.

Table of contents

1. General

2. Functional scope

3. Compatibility

4. Test Certificates

5. Components released

6. Condition on delivery of SIMOTION SCOUT / SIMOTION update contracts

1. General

SIMOTION V4.3 SP1 HF12 has been released for delivery with immediate effect. We recommend that you generally use the Version V4.3 SP1 HF12.

The release refers to the following components:

  • SIMOTION SCOUT Engineering System and SCOUT Stand-alone V4.3 SP1 HF12
  • SIMOTION Kernel/Firmware V4.3 SP1 HF12 (supplied with the SIMOTION SCOUT)

Users who have concluded a valid Software Update Service contract for SCOUT and SCOUT Stand-alone are automatically supplied with SIMOTION SCOUT/SCOUT Stand-alone V4.3 SP1 HF12 (delivered on DVD).
All licenses for SCOUT V4.3 remain valid.

With immediate effect, the Control Units SIMOTION D4xx and D4xx-2 with Software Version V4.3 SP1 HF12 have been released. The CF cards for SIMOTION D4xx (6AU1400-2PA02-0AA0), SIMOTION D410-2 (6AU1400-1PA22-0AA0) and SIMOTION D4x5-2 (6AU1400-2PA22-0AA0) are delivered with SIMOTION Kernel V4.3 SP1 HF12.

The SIMOTION C240/C240 PN with Software Version V4.3 SP1 HF12 has been released with immediate effect. The MMC card for SIMOTION C240/C240 PN (6AU1720-1KA00-0AA0) is delivered with SIMOTION Kernel V4.3 SP1 HF12.

With immediate effect, the SIMOTION P320-3 and SIMOTION P350-3 with Software Version V4.3 SP1 HF12 have been released.
SIMOTION P320-3 will continue to be supplied ex factory with SIMOTION Kernel V4.3 SP1 HF1. The Kernel V4.3 SP1 HF12 will be provided on the SCOUT DVD and can be used to upgrade the SIMOTION P320-3 to the Version V4.3 SP1 HF12.
SIMOTION P350-3 will continue to be supplied ex factory with SIMOTION Kernel V4.3 SP1 HF3. The Kernel V4.3 SP1 HF12 will be provided on the SCOUT DVD and can be used to upgrade the SIMOTION P350-3 to the Version V4.3 SP1 HF12.

2. Functional scope

With SIMOTION V4.3 SP1 HF12, various functional limitations applying in the Engineering System and Runtime Kernels have been eliminated. After installing the SINAMICS Support Package "SSP SINAMICS V4.6“, you can use SINAMICS V4.6 with SINAMICS S120 CU310-2 resp. CU320-2.

The setup of SIMOTION SCOUT and SCOUT Stand-alone V4.3 SP1 HF12 is a complete setup (no delta setup), that means, the installation duration corresponds to the duration of a new installation.

3. Compatibility

SIMOTION SCOUT Version V4.3 SP1 HF12 is compatible with the Versions V4.2, V4.1, V4.0 and V3.2.

Projects which have been created with older versions can

  • be upgraded to the new version (e.g. if the existing project shall be extended by functions included in the Version V4.3 SP1 HF12). The relevant description is included in the Readme resp. the manual.
  • also be processed with the SCOUT Version V4.3 SP1 HF12 (only the project data are converted upwards, Runtime remains unchanged). If necessary, you can afterwards store the project data in the format V4.2, V4.1, V4.0 and V3.2. Projects which have been created unter V3.0 or V3.1 must be upgraded before to the Version V3.2 (or later) using an older SCOUT version.

The current SIMOTION compatibility list with the software and hardware combination is provided at 18857317.

Note regarding the TopLoading Application

The Toploading Application V1.9 is required when using the TopLoading Application with SIMOTION V4.3 SP1 HF12. Due to various interface modifications, the Application Version V1.8 is no longer supported as from SIMOTION V4.2 SP1.

4. Test Certificates

In general, the SINAMICS Safety Integrated functions provided by SINAMICS/SIMOTION are certified by independent institutes. A list of currently certified components is available on request from the regional Siemens office. If you have any questions regarding certifications which have not been completed so far, please contact your local Siemens contact person.

The SIMOTION D CompactFlash Cards are supplied with Kernel/Firmware V4.3 SP1 HF12 and SINAMICS Integrated drive software.

SIMOTION D Kernel/Firmware Versions V4.3 SP1 HF12

SINAMICS Integrated drive software version V2.6 SP2 HF17
(V02.60.45.27)
V4.5 HF14
(V04.50.30.19)
Firmware Version "Safety Integrated Basic Functions"

V02.60.40.00 (CU)

V02.60.40.00 (P2, only with D410)

V04.50.30.05 (CU)

V04.50.30.05 (P2, only with D410-2)

Firmware Version "Safety Integrated Extended Functions"

V02.60.45.13 (CU)

V02.60.45.03 (P2, only with D410-2)

V04.50.30.14 (CU)

V04.50.30.14 (P2, only with D410-2)

Control Units supported D410, D425, D435, D445-1, CX32 D410-2, D425-2, D435-2, D445-2, D455-2, CX32-2

The current status of the available certificates complying with international standards and machine safety regulations (TÜV, BGIA) is provided at the following link: http://support.automation.siemens.com/WW/view/de/13305690/134200.

5. Components released

SIMOTION SCOUT

Order numbers Designation Version
6AU1810-1BA43-1XT7 SIMOTION Engineering System SCOUT V4.3 SP1 HF12 DVD, Demo/Trial Version with Trial License V4.3 SP1 HF12
6AU1810-1CA43-1XT7 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF12 DVD, Demo/Trial Version with Trial License V4.3 SP1 HF12
6AU1810-1BA43-1XA0 SIMOTION Engineering System SCOUT V4.3 SP1 HF12 DVD, with Full License (Floating License) V4.3 SP1 HF12
6AU1810-1BA43-1XE0 SIMOTION Engineering System SCOUT V4.3 SP1 HF12 Upgrade DVD, with Upgrade License V4.3 SP1 HF12
6AU1810-1CA43-1XA0 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF12 DVD, with Full License (Floating License) V4.3 SP1 HF12
6AU1810-1CA43-1XE0 SIMOTION Engineering System SCOUT Stand-alone V4.3 SP1 HF12 Upgrade DVD, with Upgrade License V4.3 SP1 HF12

SIMOTION D

Order numbers Designation Version/note
6AU1400-2PA02-0AA0 CompactFlash Card (CF) 1 Gbyte for SIMOTION D4xx
with SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be prelicensed via Z-options

Note: Only for SIMOTION D4xx

V4.3 SP1 HF12

(SINAMICS V2.6 SP2 HF17)

6AU1400-2PA22-0AA0 CompactFlash Card (CF) 1 Gbyte for SIMOTION D4x5-2
with SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be prelicensed via Z-options

Note: Only for SIMOTION D4x5-2

V4.3 SP1 HF12

(SINAMICS V4.5 HF14)

6AU1400-1PA22-0AA0 CompactFlash Card (CF) 1 Gbyte for SIMOTION D410-2
with SIMOTION Kernel/Firmware and SINAMICS S120 drive software; current software version; can be prelicensed via Z-options

Note: Only for SIMOTION D410-2

V4.3 SP1 HF12

(SINAMICS V4.5 HF14)

Notes The Firmware V4.3 SP1 HF12 is included in the scope of delivery of SIMOTION SCOUT. Further, the Firmware can be downloaded from the Product Support, see 31045047.

SIMOTION D445 with order no. "6AU1445-0AA00-0AA0" is no longer supported as from Runtime System V4.3. However, with SCOUT V4.3, the Control Unit can still be configured with Runtime System < V4.3. 

SIMOTION C

Order numbers Designation Version/Note
6AU1720-1KA00-0AA0 MMC 64MB for SIMOTION C240 / C240 PN with SIMOTION Kernel/Firmware; can be prelicensed via Z-options V4.3 SP1 HF12
Notes The Firmware V4.3 SP1 HF12 is included in the scope of delivery of SIMOTION SCOUT. The Firmware can be downloaded from the Product Support, see 31263919.

The C230-2 with order no. "6AU1230-2AA01-0AA0" is no longer supported as from Runtime System V4.2. However, with SCOUT V4.3, it can still be configured with Runtime System < V4.2.

SIMOTION P

Order numbers Designation Version/Note
6AU1350-3AK41-1BE2 - Z V43 W01 SIMOTION P350-3 PROFIBUS, Pentium M 2GHz, without DVD-ROM

SIMOTION P350-3 will continue to be delivered ex factory with SIMOTION Kernel V4.3 SP1 HF3. The Kernel V4.3 SP1 HF12 is provided on the SCOUT DVD and can be used to upgrade the SIMOTION P350-3 to the Version V4.3 SP1 HF12.

 

SIMOTION P320-3 will continue to be delivered ex factory with SIMOTION Kernel V4.3 SP1 HF1. The Kernel V4.3 SP1 HF12 is provided on the SCOUT DVD and can be used to upgrade the SIMOTION P320-3 to the Version V4.3 SP1 HF12.

 

 

 

 

6AU1350-3AK43-1BE2 - Z V43 W01 SIMOTION P350-3 PROFIBUS, Pentium M 2GHz, with DVD-ROM
6AU1350-3AK41-2BE2 - Z V43 W01 SIMOTION P350-3 PROFINET, Pentium M 2GHz, without DVD-ROM
6AU1350-3AK43-2BE2 - Z V43 W01 SIMOTION P350-3 PROFINET, Pentium M 2GHz, with DVD-ROM
6AU1320-7AB55-3AF0 SIMOTION P320-3 PROFINET, INTEL CORE 2 SOLO 1.2 GHZ with WINDOWS EMBEDDED STANDARD 2009

Device Update Tool/Firmware Support Package

With the Device Update Tool for upgrading SIMOTION devices, SIMOTION provides a user-friendly solution. The Firmware Support Package V4.3 SP1 HF12 is included in the scope of delivery of SIMOTION SCOUT. For SIMOTION D and SIMOTION C, the  Firmware Support Package can also be downloaded from the Product Support, see 33119786.

6. Condition on delivery of SIMOTION SCOUT / SIMOTION SCOUT update contracts

SIMOTION SCOUT

The Version V4.3 SP1 HF12 replaces the current SCOUT and SCOUT Stand-alone V4.3 SP1 HF3 versions delivered. Thus, when ordering software, only the Version 4.3 SP1 HF12 will be delivered.

The SIMOTION SCOUT Version V4.3 SP1 HF12 requires the version STEP7 V5.5 SP2 or V5.5 SP3 as option package for STEP7. SCOUT Stand-alone V4.3 SP1 includes the STEP7 components of the Version V5.5 SP2. SCOUT and SCOUT Stand-alone have been released for the operating systems Windows XP Professional SP3 resp. Windows 7 / Windows 7 SP1 Professional and Ultimate (32 and 64 bit).

SIMOTION SCOUT software versions must be ordered stating the above-stated order numbers.

Important note:
The existing automatic substitution to the current version delivered in case of new orders placed for older versions does no longer apply. Thus, spare parts need no longer be ordered when purchasing older versions.
As the Version 4.3 SP1 HF12 replaces the previous version delivered, the previous Hotfix Versions for V4.3 can no longer be ordered.

SIMOTION SCOUT update contracts

Users who have concluded a valid Software Update Service contract for SCOUT or SCOUT Stand-alone are automatically supplied with SCOUT or SCOUT Stand-alone V4.3 SP1 HF12 (delivered on DVD). Users who have not concluded an update service can order the current software version stating the above-stated order numbers.

For more detailed information, please contact your local Siemens office.

SINAMICS Support Package

If you wish to use the SINAMICS V4.6 with SIMOTION SCOUT V4.3 SP1 HF12, you must install the SINAMICS Support Package "SSP SINAMICS V4.6". The SSP is provided on the SIEMENS Industry Online Support pages under /cs/document/26233208?caller=view&lc=de-WW

The information section "SINAMICS MICROMASTER STARTER V4.3 SP1 HF2/HF5 (previous version)" includes a table listing the download files of the individual SSPs:

  • SSP, SINAMICS G120 V4.6: SSP_SINAMICS_G120_V4_6.zip
  • SSP, SINAMICS MV V4.6: SSP_SINAMICS_MV_V4_6.zip
  • SSP, SINAMICS S120, G150, G130 V4.6: SSP_SINAMICS_V4_6.zip
  • Online Help: Vol_3_STARTER_V43_SP2_HELPS.zip

Important note:
The SINAMICS Integrated for SIMOTION D4xx-2 remains V4.5.
SINAMICS V4.6 drive functions, which require, in addition to the new SSP parameter description, also the newer STARTER Version V4.3 SP2, will only be provided with the next SIMOTION full version.

SIMOTION CamTool

The Software CamTool V3.0 SP2 is included in the complete SCOUT or SCOUT Stand-alone package, the necessary license must be ordered separately. Existing CamTool V3.0 licenses remain valid. Licenses for CamTool lower than V3.0 must be upgraded to the current Version 3.0 by ordering an upgrade (6AU1810-0FA30-2XE0).

SIMOTION DCC

The corresponding DCC SIMOTION with license must be ordered. DCC SIMOTION comprises the license for DCC SIMOTION and DCC SINAMICS. Licenses which have already been delivered for V2.1 remain valid for V2.2 SP1. Licenses V2.0 which have already been delivered require an Upgrade License. With the setup for SCOUT V4.3 SP1, the DCC libraries (DCB) are installed automatically and optionally also the DCC Editor (CFC V8.0). The orderable DCC DVD need not be installed separately.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit