×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 6836122, Entry date: 11/17/2009
(3)
Rate

What can be the cause of the message "HResult Error" in conjunction with WinCC?

  • Entry
  • Associated product(s)

Configuration Notes:
The files listed below give the HResult errors and possible causes as well as corresponding remedies for the different versions of WinCC.
These messages occur only when you open a project or start in Runtime. Even if a client logs on to a server, you can still get this message.

HResult Error WinCC V7.x and V6.x
The following file is valid for WinCC V7.x and V6.x, because the error numbers and causes/remedies are identical.

HResult Error WinCC V7.x and V6.x ( 85 KB )

 

HResult Error WinCC V5.x

HResult Error WinCC V5.x ( 33 KB )

 

File EnableDCOM.zip for HResult Error 0x80080005

EnableDCOM.zip ( 514 bytes )

Keywords:
System message, 26341426, 9126124, 16640039, 19439600, 23711489

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.