×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 68791688, Entry date: 06/12/2013
(2)
Rate

Update 1 for D7-SYS V8.0

  • Entry
  • Associated product(s)

DESCRIPTION

The Update 1 referenced below corrects the following problems:

  1. SFC Online can now be terminated without crash of the channel broker.
  2. The SFC-XML file will always be generated when selected in the options menue.

The prerequisite for the use of Update 1 is D7-SYS V8.0.

 

D7-SYS_V80_Upd1.zip ( 4831 KB )

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.