×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 69864408, Entry date: 03/15/2019
(40)
Rate

Time synchronization between an HMI and a SIMATIC PLC

  • Entry
  • Associated product(s)
Depending on the required time synchronization and the SIMATIC controller used, this article shows the appropriate solution.

Introduction
In order for components, such as HMI operator interfaces and SIMATIC controllers of a system to work with an identical time, one of the listed components must be a timer for all other components.

  • The component acting as a timer is referred to as the time master.
  • The time receiving components are the time slaves.


Fig. 01

Time synchronization is essential, for example, in the following fields of application:

  • Data recording and data storage
  • Alarms
  • Shift protocols
  • Energy data management

For a better overview, this application example is divided into three parts:

  • A guiding document is intended to give a brief overview, explain certain terms and make it easier to find existing FAQs.
  • The first example project shows the "Clock synchronization between an HMI operator interface and a SIMATIC PLC".
  • The second example project shows the "Clock synchronization between WinCC Runtime Professional and a SIMATIC PLC".

Guiding document for time synchronization

The guiding document provides an overview of clock synchronization, explains certain terms and makes it easier to find existing FAQs in this context.

  Documentation (877,1 KB)

Time synchronization between an HMI operator interface and a SIMATIC PLC

The example project shows the respective possibilities of clock synchronization and their programmatic implementation.

A distinction is made between the following synchronization types:

  • HMI clock synchronization (master)
  • HMI clock synchronization (slave)
  • Area pointer: Date/time
  • Area pointer: Date/time PLC
  • Area pointer: Control order 14 and 15

The example project deals with two tasks:

  1. For the first task, an HMI user interface is to be the timing component.
    (HMI operating unit → SIMATIC control).
  2. In the second task, a SIMATIC controller is to be the timing component.
    (SIMATIC controller → HMI operator interface).

An example project is stored for each synchronization type.

The description applies to the following SIMATIC controllers and HMI operator interfaces:

  • SIMATIC controllers
  • SIMATIC S7-1200
  • SIMATIC S7-1500
  • SIMATIC S7-300
  • SIMATIC S7-400
  • HMI operating devices
  • SIMATIC Basic Panel
  • SIMATIC Panels
  • SIMATIC Comfort Panel
  • SIMATIC Multi Panel
  • SIMATIC Mobile Panel
  • SIMATIC RT Advanced

Documentation und example projekt
  Documentation (2,0 MB)
 Registrierung notwendig  Example project for WinCC and STEP 7 V13 SP1 (39,0 MB) 


Time synchronization between WinCC Runtime Professional and a SIMATIC PLC

The clock time of a higher-level Industrial PC (time master) is transferred to all connected devices (time slaves).

The sample project covers two tasks, depending on the hardware used:

  1. The adjustment of time and date is carried out via interface variables.

  2. The time and date are compared using the NTP protocol. 

The description applies to the following SIMATIC controllers and HMI operator interfaces:

  • SIMATIC controllers
  • SIMATIC S7-1200
  • SIMATIC S7-1500
  • SIMATIC S7-300
  • SIMATIC S7-400
  • Time master
  • PC with WinCC Runtime Professional
  • IPC when using the NTP protocol

Documentation and sample project
  Documentation (1,6 MB)
 Registrierung notwendig  AWL Code for S7-300/S7-400, SCL-Code for S7-1200/S7-1500, VB-Code for WinCC Professional (1,1 KB)

Last change
Document completely revised Project planning adapted
 
Additional keywords
Adjust time, S7 300, S7 400, Control, Time, Adjust time, Area Pointer, Synchronization, Synchronize, Set, TIA Portal, STEP7, STEP 7, NTP, 67518641

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit