×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 69870640, Entry date: 05/07/2013
(1)
Rate

SINUMERIK 840D sl Safety functions: Calculation examples for an axis subject to gravitational force

  • Entry
  • Associated product(s)

Task  
Calculation examples for an axis subject to gravitational force.


Bild 01

Solution
This application example explains how to calculate the Performance Level for an axis subject to the force of gravity, based on the EN ISO 13849 standard.
The following cases are taken into consideration:

  • When the protective doors are open, an axis subject to the force of gravity is in the safe operating stop condition
  • When the protective doors are open, an axis subject to the force of gravity is traversed with an acknowledgment button and with a safely reduced velocity
  • Holding an axis subject to the force of gravity when the power fails
  • Stopping an axis subject to the force of gravity in an emergency (Emergency Stop)

Downloads

Content of Downloads

Download

Documentation 69870640_example_hanging_axis_DOKU_V11.pdf ( 1235 KB )
Calculation example (Hanging_axis_en.set, Hanging_axis.ssm) 69870640_hanging_axis.zip ( 132 KB )

Last Changes
05/2013, first publication

Additional Keywords
motioncontrol_cnc_applications, SI-Funktionen, SI Functions

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.