×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 70968313, Entry date: 10/20/2014
(25)
Rate

Why is the installation of S7 Distributed Safety V5.4 aborted in Windows 7 Enterprise/Professional 64-bit?

  • Entry
  • Associated product(s)

Description
For the installation of S7 Distributed Safety V5.4 (SP5 + Update 1 onwards)keep to the procedure described below by

  • installing first S7 Distributed Safety V5.4 and
  • then WinCC.

If you have installed WinCC before S7 Distributed Safety V5.4 or you get the error message "The wizard was aborted before S7 Distributed Safety Programming could be installed completely", proceed as follows to install in the given order.

  1. Open the Explorer in Windows 7 and mark the folder
    C:\Programs(x86)\Common Files\InstallShield\Driver\11
    Note
    Parts of the path might be hidden depending on the setting.
      

    Fig. 01
     
  2. Rename folder "11" (arbitrary name).
  3. Install S7 Distributed Safety V5.4.
    Note
    S7 Distributed Safety V5.4 now also creates a folder
    C:\Programs(x86)\Common Files\InstallShield\Driver\11.
  4. Delete the folder "11" created by S7 Distributed Safety V5.4
    C:\Programs(x86)\Common Files\InstallShield\Driver\11.
  5. Change the name of the folder changed in point 2 back to
    C:\Programs(x86)\Common Files\InstallShield\Driver\11.
    Note
    The contents of the folders "C:\Programs(x86)\Common Files\InstallShield\Driver\11" is thus restored to as it was before S7 Distributed Safety V5.4 was installed.

Additional Keywords
Safety integrated  


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit