×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 70989159, Entry date: 04/11/2014
(3)
Rate

SINUMERIK 840D, 840D sl: HUBITRON HBG 800 DP wireless handwheel

  • Entry
  • Associated product(s)

Task & Solution
The application describes the connection of the HUBITRON HBG 800-DP and HBG 800-DP FS wireless handwheels to a SINUMERIK 840D sl, as well as their operation.
Because this application can be used for both handwheel types as well as the SINUMERIK 840D sl, 840D, 840Di sl and 840Di controller types, only the HBG 800-DP and SINUMERIK 840D sl types are mentioned in the subsequent description.
In the application example, the HBG 800-DP emulates partially the buttons on the MCP310/MCP483 machine control panel (MCP).
The assigned buttons of the HBG 800-DP front foil supplied from HUBITRON are supported in the application. The free foil buttons are used as follows:

  • Button 4 selects axis 4
  • Button 16 selects axis 5 and further axes
  • Button 8 is assigned for the channel selection
  • Button 15 switches between the workpiece-related and the machine-related position display
  • Button 14 switches between the workpiece- and the machine-coordinate system

Note
If you are interested, please contact your local sales partner.
Contacts worldwide

Downloads

Content of downloads

Download

Documentation 70989159_HBG800-DP_Doku_V20_en.pdf ( 1608 KB )

Last Changes
04/2014

Additional keywords
motioncontrol_cnc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.