×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 72840622, Entry date: 03/16/2017
(4)
Rate

SINAMICS S120 1:1 Synchronism with DCC

  • Entry
  • Associated product(s)
Camming permits relative motion between a leading and following axis with the correct angle, which can be implemented using freely parameterizable cams. This replaces mechanical eccentric cams and cranks.

Note: For this application example, there is already a newer version available 109757232


Task
In synchronous operation, the axis is externally controlled as following axis. The position setpoint is derived from a leading axis (master value source). In the synchronous operation mode, many axes can be coupled, which are either all controlled from the same leading axis or in groups of various leading axes.

Solution
This application solves the task by means of the blocks from the GMC library. The GMC library is based on SINAMICS DCB Extension and is an extension for the existing DCC standard library. With the new motion control blocks, application function can be realized drive based in SINAMICS S120.

The synchronism application includes the following functions:

  • Real leading axis
  • Virtual leading axis
  • Synchronization to master value
  • Absolute and relative offset input
  • Flying homing for following axis and real leading axis
  • Homing for following axis and real leading axis
  • Positioning for the real and virtual leading axis
  • Deadtime compensation
  • Following error monitoring


Additional search terms
motioncontrol_apc_applications


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.