×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 73016883, Entry date: 12/21/2018
(8)
Rate

PROFIBUS GSD files: ET 200SP

  • Entry
  • Associated product(s)
Download: PROFIBUS GSD files for ET 200SP

Station type: IM 155-6 DP HF V4.2 (Rev.5)
Order no.: 6ES7 155-6BU01-0CN0
Version: 10/2018
 Registrierung notwendig  ET200SP_DP_HF_V42.zip (185,6 KB)
SHA256 checksum: 9F95625E85B29902C951007EAA6F06CE577B2E1CDD0DC04ABD149398488FBBAD

Station type: IM 155-6 DP HF V3.1 (Rev.5)
Order no.: 6ES7 155-6BU00-0CN0
Version: 08/2018
 Registrierung notwendig  ET200SP_DP_HF_V31.zip (179,8 KB)
SHA256 checksum: 152C7050E634349DD0A76D0A896D55F06B455D24B6CA9F34E7DA6BA52FF938E2

Station type: IM 155-6 DP HF V1.1 (Rev.5)
Order no.: 6ES7 155-6BU00-0CN0
Version: 02/2014
 Registrierung notwendig  et200sp_dp_hf_v11.zip (68,7 KB)
SHA256 checksum: 78F097D5B313294DCACAA4DA29472189B51CC75759CA8772D3CF835922D78167

Station type: IM 155-6 DP HF V1.0 (Rev.5)
Order no.: 6ES7 155-6BU00-0CN0
Version: 08/2013
 Registrierung notwendig  et200sp_dp_hf.zip (21,6 KB)
SHA256 checksum: 6C46233B17C707E1D3927E964C4284DD53090F09FB18BEC361E7812A805A9A04

Station type: IM 155-6 DP HF V4.2 (Rev.3)
Order no.: 6ES7 155-6BU0x-0CN0
Version: 10/2018
 Registrierung notwendig  ET200SP_DP_HF_V42_Rev3.zip (155,7 KB)
SHA256 checksum: A0C4A83A8BF9F2763BBA5E6AE5D75BD2626CC25766CEA0A27C01808EF5435890

Station type: IM 155-6 DP HF V3.1 (Rev.3)
Order no.: 6ES7 155-6BU00-0CN0
Version: 08/2018
 Registrierung notwendig  ET200SP_DP_HF_V31_Rev3.zip (151,1 KB)
SHA256 checksum: 6784B1AB83547B7677D3835445EAC54952E7209986047D06566DA4617C4481D2

FAQ: How do you determine the SHA-256 checksum of a file? 109483101 

New PROFIBUS GSD file revision 3 for ET 200MP and ET 200SP

An additional GSD file in revision 3 is now available in addition to the previous PROFIBUS GSD files with revision 5


Using the GSD files

  • This GSD file is only to be used if the configuration cannot be done using the GSD file revision 5.
  • The revision 3 GSD files can be used with all engineering tools that do not support the revision 5 GSD files e.g. COM PROFIBUS. There are also many older engineering tools that do not allow the installation of newer GSD files because they contain newer key words.
  • These GSD files now allow the ET 200 MP and ET 200SP modules to be used on PROFIBUS master modules that do not support DP V1 operation with data records. Naturally, in this case, all functions based on data record communication cannot be used.

 

Note

 

  • Due to the functional limitations of a number of engineering tools, when these GSD files are used certain module parameters are available for selection that the modules do not support.
  • For example for an AQ 4xU/I ST (6ES7 532-5HD00-0AB0) an output range of +/- 5V can be configured. The module does not support this, however. When a parameter assignment of this type is downloaded to this module, the module shows a parameter assignment error. For this reason please note which parameters the module supports in the device manual for each module.
  • This GSD file is not suitable for the DP master configuration of a AG 95U due to its limited address volume.

 

 

 

Download

You can download the revision 3 GSD files here:

ET 200SP: 73016883

ET 200MP: 80206700

 

You can download the manuals (Manual Collection) for the ET 200 MP and ET 200SP here:

Manual Collection ET 200MP: 86140384

ET 200SP Manual Collection 84133942