×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 73158403, Entry date: 05/15/2013
(1)
Rate

How do you read out the GSM/GPRS signal quality of the CP 1242-7 via the S7-1200 CPU?

  • Entry
  • Associated product(s)
The S7-1200 CPU uses the Read Record function to read out the GSM/GPRS signal quality of the CP 1242-7 and store it in a DB.

Requirements
CP 1242-7 firmware version V1.2 or higher

Note
This FAQ response is not valid for CP 1242-7 V2.

Instructions
To use this function you follow the procedure described in the table below:
 

No. Procedure
1 Create a DB with a structure tag as explained below: 
   


Fig. 01

2 Call RDREC cyclically in OB1 with the following parameters:

REQ = TRUE (to transfer the data record)
ID = Hardware identifier of the CP (go to Device Configuration and select the CP 1242-7 > Properties > Hardware Identifier)
INDEX = 12336 (data record number; 12336 for the GPRS signal quality)
MLEN = 12 bytes (maximum length of the data record data to be read)
RECORD = pointer to the data record in the DB created in step 1. 
   


Fig. 02

3 Click "Go online" and use the the "Monitor all" function to read the value of the "Signal quality" tag.
   


Fig. 03

Table 01

The values and their meanings for this tag are given in the table below:

Value Meaning Comments
0 GOOD -73… > -53 dBm
1 UNSTABLE -89… -75 dBm
2 WEAK -109… -91 dBm
3 NO_SIGNAL < -111 dBm
Table 02

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.