×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 7388266, Entry date: 05/02/2001
(0)
Rate

Missing DLL after installation of Softnet IE from the SIMATIC NET CD (release 5/2000) with WinAC Slot V3.1

  • Entry
  • Associated product(s)

QUESTION:
Why doesn't my WinAC Slot V3.1 (412/416-PCI) work, although I have installed the Softnet IE driver from the SIMATIC NET CD?

ANSWER:
You are using a WinAC Slot V3.1 (412/416-PCI) and have installed the "Softnet IE" driver for your Ethernet card from the SIMATIC NET CD (at least 05/2000), but a DLL for the driver has not been installed. To install this DLL you must install the driver "S7 1613" from the SIMATIC NET CD. This installation adds the necessary TCP driver.

Keywords:
Driver update, Function extension


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.