×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 74747848, Entry date: 09/27/2018
(0)
Rate

PCS 7 Unit Template "Dryer" using the example of the Chemical Industry

  • Entry
  • Associated product(s)
The unit template "Dryer" is based on a standardized and structured design of the automation program through the use of predefined equipment and control modules. The example is used both as a basis for projects and as an overall standardization template.
Task
The standardization of automation engineering for processing plants, such as in the chemical industry, is a major challenge. Different process steps and procedures, different equipment and flexibility in the production make the task even more difficult.
This includes the structuring of the plant according to the physical model of the DIN EN 61512 standard. This specifies the lower four levels, i.e. plant, unit, technical facility and control module. A plant always consists of units. The units can, in turn, comprise technical facilities which can be automated by equipment modules.

Solution
This application example presents a fluidized bed dryer, with which the energy consumption can be optimized by using an MPC (Model Predictive Control) controller. Drying operations require a high amount of energy, which is why optimum and economical drying (as dry as necessary) is the objective.

Over-drying wastes energy and reduces the weight of the product, which can possibly negatively affect the sales revenue (based on weight). Insufficient drying, on the other hand, can cause difficulties in downstream process stages, e.g. decay, mold, lumps, etc. Therefore, precise controlling of the particle moisture content has great economic significance.

The unit template "Dryer" provides a template that comprises all typical components, their open- and closed-loop control, the necessary logic and interlocking as well as the visualization. It is modularly structured and based on standardized equipment modules and process tag types.

Its utilization offers the following advantages:

  • A reduction of the knowledge necessary to develop applications
  • A decrease in the configuration effort
  • More flexible setup and adaptation due to equipment modules
  • Standardized structures

Equipment Modules and Unit Templates
Efficient Engineering with SIMATIC PCS 7 in the Chemical Industry


Validity

  • SIMATIC PCS 7 V9.0 SP1
  • SIMATIC PCS 7 V8.0 SP1

Documentation and Sample Project for PCS 7 V9.0 SP1
  Documentation (2,4 MB)
  Show mobile friendly
You can download the example project for PCS 7 V9.0 SP1 in the Extranet-section of this entry. This Extranet section is only visible if have concluded a Managed System Services contract. Refer to the following link for detailed information: Managed System Services.

Documantation and Sample Projects for PCS 7 V8.0 SP1
  Documentation (4,2 MB)
 Registrierung notwendig  PCS 7 V8.0 SP1 sample project (118,4 MB)

Further Information
Equipment Modules for PCS 7 using the example of the Chemical Industry
PCS 7 Unit Template "Distillation Column" using the example of the Chemical Industry
PCS 7 Unit Template “Stirred Tank Reactor” using the example of the Chemical Industry
PCS 7 Unit Template "Fermenter" using the example of the Chemical Industry
PCS 7 Unit Template “Polymerization Reactor” using the example of the Chemical Industry
Integration of Advanced Process Graphics in SIMATIC PCS 7
Simulation of a PCS 7 stirred tank reactor with SIMIT Simulation Framework
Service Contracts - SIMATIC PCS 7 Lifecycle Services

Last Changes
Update for PCS 7 V9.0 SP1 with Integration of Smart Alarm Hiding

Additional Keywords
E-Learning, Tutorial, Teaser, Webcast, Multimedia-based demonstration system, MMDS, Film, Screencast, contact dryer,convection dryer, dry air, drying process

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.