×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 75277515, Entry date: 07/30/2013
(22)
Rate

Service Pack 1 for SIMATIC STEP 7 V12 (TIA Portal) incl. PLCSIM

  • Entry
  • Associated product(s)

The Service Pack is applicable to the following products:

  • STEP 7 Professional V12
  • STEP 7 Basic V12

New features and changes compared to earlier versions are described in the delivery release for STEP 7 V12 SP1: entry ID 76276623 

 

Installation instructions:

Installation of the Service Pack requires prior installation of the STEP 7 V12 software.

 

The TIA Portal products STEP 7 (incl. PLCSIM), WinCC and Startdrive must be updated to the same version (V12 SP1). If the versions differ, the TIA Portal can no longer be started. Please ensure that you have the Service Packs for these products on hand before you begin with the installation. The Service Packs are available from the following entry IDs:

 

Instructions for the download 

The download is divided into several files. Please download all the files into the same directory and execute the file ending with .exe. The files will now be combined and you can execute the setup.

 

 

Service Pack 1 for STEP 7 V12 Professional incl. PLCSIM

SIMATIC_STEP_7_Professional_SP1_for_V12.exe (2653 KB) ( 2653 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.001 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.002 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.003 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.004 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.005 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.006 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.007 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Professional_SP1_for_V12.008 (75593 KB) ( 75593 KB )
  SIMATIC_S7_PLCSIM_V12_SP1.exe (1520508 KB) ( 1520508 KB )

 

 

Servicepack 1 für STEP 7 V12 Basic

 

SIMATIC_STEP_7_Basic_SP1_for_V12.exe (2653 KB) ( 2653 KB ) ( 2653 KB )
  SIMATIC_STEP_7_Basic_SP1_for_V12.001 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V12.002 (665600 KB) ( 665600 KB )
SIMATIC_STEP_7_Basic_SP1_for_V12.003 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Basic_SP1_for_V12.004 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Basic_SP1_for_V12.005 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Basic_SP1_for_V12.006 (665600 KB) ( 665600 KB )
  SIMATIC_STEP_7_Basic_SP1_for_V12.007 (317953 KB) ( 317953 KB )

 

 

 

 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.