×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 75407031, Entry date: 03/26/2017
(3)
Rate

SIMATIC PCS 7 CPU 410-5H Process Automation Released for Delivery

  • Entry
  • Associated product(s)
The CPU 410-5H Process Automation is an exclusive product for the SIMATIC PCS 7 process control system and is herewith released for delivery. This CPU enables a very flexible scaling of the modular SIMATIC PCS 7 automation systems AS 410; it can be employed in all domains, i.e. as standard automa...

The CPU 410-5H Process Automation is an exclusive product for the SIMATIC PCS 7 process control system and is herewith released for delivery. This CPU enables a very flexible scaling of the modular SIMATIC PCS 7 automation systems AS 410; it can be employed in all domains, i.e. as standard automation system AS 410S, as fault-tolerant automation system AS 410H and as failsafe automation system AS 410 F/FH.

1 Product Information and Ordering Data

Product information and technical data of the CPU 410-5H Process Automation as well as information and ordering data of the automation systems AS 410S, AS 410H, AS 410F and AS 410FH which can be configured with this CPU are provided under "Modular Systems S7-400" in the chapter "Automation Systems" of the Catalog ST PCS 7, edition June 2013.

 stpcs7_K09_en.pdf (1095 KB) ( 1389 KB )  (capital 09; english )


Two online configurators for the interactive configuration of the AS-Bundles AS 410S AS 410H, AS 410F and AS 410FH  in the Industry Mall (http://www.siemens.com/industrymall) are in preparation:

  • Configurator SIMATIC PCS 7 AS 410 Single Station
  • Configurator SIMATIC PCS 7 AS 410 Redundancy Station

We will inform you as soon as they become available.

2 Compatibility

The CPU 410-5H Process Automation is based on innovated hardware with operating system V8.0. The operating system V8.0 can only run on this innovated hardware. The hardware of the S7-400-CPUs V6.0 cannot be upgraded.

For the configuration of the CPU 410-5H Process Automation you require the engineering software SIMATIC PCS 7 V8.0+SP1 and the Hardware Upgrade Package HUP CPU410-5H (see Download entry ID 68627630). Loading of application software blocks is only possible with the SIMATIC PCS 7 engineering software. Attempts to load via the SIMATIC Manager or a STEP 7 editor (e.g. STL editor) will be rejected by the CPU.

With respect to the application programs the CPU 410-5H Process Automation is compatible with the predecessors. This means that you can reuse the existing charts with a new compilation using the current Basis Library (min. V8.0 SP1 Upd1). The hardware configuration, on the other hand, must be newly created.

No external PROFINET interface modules can be used in automation systems with the CPU 410-5H Process Automation

3 Replacement Strategy

The CPU 410-5H Process Automation will supplement the existing product spectrum. It can be employed in systems with SIMATIC PCS 7 V8.0+SP1 (incl. HUP) as standard controller and as failsafe or fault-tolerant controller for SIMATIC PCS 7 automation systems AS 410. For SIMATIC PCS 7 systems with SIMATIC PCS 7 V6 or V7 we will continue to offer PCS 7 AS Bundles with S7-400 CPUs V6.0.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.