×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 75735742, Entry date: 07/02/2013
(0)
Rate

Low-voltage converters SINAMICS G150 (6SL3710-xxxx-xxx3) – Change notification for various options

  • Entry
  • Associated product(s)

As a result of changed general conditions and requirements, several options of the SINAMICS G150 cabinet unit will be changed or new options released.

CHANGE: Option K74 "230 V AC auxiliary power supply"

Up until now, for all SINAMICS G150 cabinet units, only one 230V AC power supply was installed if this was internally required for options. Further, the internal 230V supply was only used in very few cases, as the control voltage is generally externally supplied.

With option K74, a 230V AC supply is integrated in the control cabinet, which supplies the internal 230V components from the power supply.

The following constellations require 230V:

G150 HP and G150 12 pulse / parallel connection / 6SL3710-2xxx

G150 6 pulse / single connection / 6SL3710-1xxx with options L13, L26 >800A, B00, G61, K50, L57, L59, L60, L83, L84, L86, L87 

For these devices and/or devices with these options, option K74 must always be ordered if there is no 230V supply.

The option can only be selected for version A (standard). Cannot be selected for version C (especially compact design). 

 

 

Example of a device circuit diagram; in future, the components marked in red, must be ordered as option K74.

The changes will come completely into effect September 30, 2013; we would ask you to take into account that all converters supplied from October 1, 2013, will reflect these changes.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.
Support to the statistics
With this function the IDs found are listed according to number (format .txt).

Generate list
Copy URL
Display page in new design
mySupport Cockpit