×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 75854607, Entry date: 05/31/2018
(8)
Rate

SITOP UPS Manager for SITOP UPS1600

  • Entry
  • Associated product(s)
With the SITOP UPS Manager you configure the SITOP UPS1600 uninterruptable power supply when connected with USB or industrial Ethernet (PROFINet).

Depending on the installed version of firmware, a specivic of the SITOP UPS manager is needed.

Firmware version of the SITOP UPS1600 Compatible SITOP UPS Manager version File

≥ V2.0.0

SITOP UPS Manager 4.72.2

 Registrierung notwendig  Setup_SITOP-UPSManager_4-72-2.zip (43,4 MB)

Do you know the current firmware release of your SITOP UPS1600?
  Instruction (173,0 KB) to determine the firmware release of a SITOP UPS1600


Procedure

  1. Save the .zip file and unpack it to a local directory.

  2. Open the local directory and follow the instructions in "EN_Read me Installation SITOP UPS Manager".

  3. For start-up of the SITOP UPS1600 with the SITOP UPS Manager please refer to
    "EN_Getting_Started_UPS1600_UPS_Manager" which is also included in the download.


Previous version sof SITOP UPS Manager:   

Firmware version of the SITOP UPS1600 Compatible SITOP UPS Manager version File

 ≥ V2.0.0 SITOP UPS Manager 4.71.15  Registrierung notwendig  Setup_SITOP-UPSManager_4-71-15.zip (43,4 MB) 

≤ V1.22

SITOP UPS Manager 4.12.5

 Registrierung notwendig  en_setupsitopupsmanager_4_12_5.zip (15,2 MB)

Please note:
For an update of firmware version V2.1.x to V2.2.0 the SITOP UPS Manager from version 4.72.2 must be used!

Do you know the current firmware release of your SITOP UPS1600?
  Instruction (173,0 KB) to determine the firmware release of a SITOP UPS1600



Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.