×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 76254308, Entry date: 01/11/2018
(11)
Rate

SINAMICS, SIMOTION, SINUMERIK, SIMOTICS: Safety functions PFH/PFD - values

  • Entry
  • Associated product(s)
In accordance with IEC 61508, IEC61511, IEC 62061 and ISO 13849-1, failure probabilities in the form of a PFH/PFD value (Probability of Failure per Hour/ Probability of Failure on Demand) have to be indicated for safety functions.

You will find the actual values of SINAMICS, SIMOTION, SINUMERIK and SIMOTICS in this document. This document is not independent; it may only be used as a supplement to the "SINUMERIK 828D / SINAMICS S120 Safety Integrated", "SINUMERIK 840D sl / SINAMICS S120 Safety Integrated", "SINAMICS S120 Safety Integrated" or "SINAMICS G120 Safety Integrated" Function Manuals.
The determination of the total PFH value of different safety functions in drive and control systems are illustrated using various examples.

You can find the actual PFH values in our "Safety Evaluation Tool" (SET):
www.siemens.com/safety-evaluation-tool

In the attachment you can find the SET project with all the examples described in the document. The examples consider IEC62061 and ISO13849-1. After loading the project in SET the examples can be used as pattern for the design of safety projects with our drives and controls.

Downloads

Content of downloads

Documentation   probability_of_failure_sinamics.pdf (731,8 KB) 

Calculation example  Registrierung notwendig  probability_of_failure_sinamics_en.zip (129,6 KB) 

Last Changes
01/2018, Updated documentation, Extension of devices

Additional search terms
SI Functions

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.