×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 76308823, Entry date: 07/02/2013
(1)
Rate

SIMOTICS: Subsequently install brake in motors for Motion Control

  • Entry
  • Associated product(s)

Summary
The retrofiting of MC motors without brake to motors with brake is uneconomic.

Question
How can a brake be subsequently installed on a motor without brake?

Answer
In general, a brake can be installed, which, however, entails large expenditure.
The following are required:  

  • New rotor

  • New bearing shield

  • Brake

  • New ball bearing

That means, in many cases retrofitting is uneconomic.

You can request a retrofit order at the following E-Mail address:

sparemotor.nes.mc.aud@siemens.com

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.