×
Siemens Industry Online Support
Siemens AG
Entry type: Product note Entry ID: 76486362, Entry date: 07/18/2013
(0)
Rate

Hotfix 02.01.00.05 for MCIS TPM SW Version 02.01.00.00, June 2013

  • Entry
  • Associated product(s)

The Hotfix 02.01.00.05 is an update for the MCIS TPM Software Version 02.01.00.00 (or later).

 

Changes included in SW 02.01.00.05 compared to SW 02.01.00.03:

  • The traffic light is updated when the connection to the database is interrupted
  • The problems arising when changing the current user TPM have been eliminated with TPMCfg
  • The component designation may comprise more than 40 characters (maximally 255 characters)

  • A message is output when the TPM cannot establish a database connection and is terminated

  • The password is changed in the login dialog

  • Problems occur when activating the alarm server with TPM IFC

  • Problems occur when executing the function Copy activity under the TPM interface Cell/HMI

  • The function Delete / archive completed activity is not correctly executed

  • Various screen fields have been enlarged on account of the foreign languages

  • Plant image as start screen

  • Following a longer plant standstill, the traffic light status and the display are not correct

Note

The originally announced Hotfix 4 is skipped because a customer-specific release has been issued.

The installation is not mandatory and necessary only if required.

We would like to draw your attention once more to the announced discontinuation of TPM (63949443)

This product version will no longer be updated !

Installation requirements

This software may only be installed on MCIS TPM SW 02.01.00.00 (or higher). On PCUs, HMI-Adv V06.04.32.08 (or higher) must be installed.

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.