×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 77317911, Entry date: 08/19/2013
(20)
Rate

SIMATIC STEP 7 V12 Trial Download (incl. SP1 and PLCSIM)

  • Entry
  • Associated product(s)

As a registered customer you can download the Trial for SIMATIC STEP 7 Professional V12 incl. Service Pack 1 and test it for 21 days. The Professional Edition also comprises the functions of SIMATIC STEP 7 Basic.

 

New features and changes compared to earlier versions are described in the delivery release for STEP 7 V12 SP1: 76276623

 

You are already using STEP 7 V12?

If you are using STEP 7 V12 already you can simply download the Service Pack 1 instead of the Trial. See entry ID: 75277515 

 

Instructions for the download:

The Trial-software is subject to export restrictions; the download is only available to registered users.

The download is divided into several files. Please download all the files into the same directory and execute the file ending with .exe. The files will now be combined and you can execute the setup.

 

 

STEP 7 Professional V12 SP1 incl. PLCSIM V12 SP1 Trial:  

 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.exe (2653 KB) ( 2653 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.001 (540490 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.002 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.003 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.004 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.005 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.006 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.007 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Professional_V12_SP1.008 (75592 KB) ( 75592 KB )
 Download unterliegt Exportkontrolle SIMATIC_S7_PLCSIM_V12_SP1.exe (1520508 KB) ( 1520508 KB )

  STEP 7 Basic V12 SP1 Trial:  

 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.exe (2653 KB) ( 2653 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.001 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.002 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.003 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.004 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.005 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.006 (665600 KB) ( 665600 KB )
 Download unterliegt Exportkontrolle SIMATIC_STEP_7_Basic_V12_SP1.007 (317953 KB) ( 317953 KB )
 

Important installation instructions:

The TIA Portal products STEP 7 (incl. PLCSIM), WinCC and Startdrive must be updated to the same version (V12 SP1). If the versions differ, the TIA Portal can no longer be started. Please ensure that you have the Trials or Service Packs for these products on hand before you begin with the installation. You can download the Service Packs here:



 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.