×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 77467239, Entry date: 07/26/2019
(14)
Rate

Transforming warning and error messages of a SINAMICS drive with the aid of the XML parser and integrating them into a STEP 7 / HMI project

  • Entry
  • Associated product(s)
The SINAMICS XML Parser supports you in displaying SINAMICS error messages in plain text directly on your HMI operator panel.

XML files with the possible warning and error messages of the respective drive are available for SINAMICS drives. These XML files that are supplied with the drive’s firmware also include these messages in plain text.
To allow easy and effective use of this information from the XML files, for example, for visualization, this XML data must be converted to a suitable file format.

Solution
The SINAMICS XML Parser converts the warning and error codes included in the XML files and the associated texts to spreadsheet CSV format. You can import the generated CSV file into a STEP 7 text library or directly display the warning and error messages in plain text on your HMI operator panel.

Advantages
The SINAMICS XML Parser offers the following advantages:

  • Easy to use:
    Using the SINAMICS XML Parser is easy and intuitive.
  • Variable use:
    All XML files with warning and error messages of the SINAMICS drives can be read.
  • Faster diagnostics:
    Messages from SINAMICS drives are displayed in plain text, which allows you to respond faster.
  • Multiple languages:
    Warning and error messages in all languages can be combined in one file.

Installation prerequisite
One of the following software packages must be installed on the PC:

  • STEP7 V5.5 or higher
  • TIA Portal V11 or higher
  • SIMOTION Scout V4.1 or higher
  • SINAMICS MICROMASTER Starter V4.1 or higher

Microsoft .NET Framework 3.5 SP1 may be automatically installed, which requires Internet access.


Converting the XML files to CSV files with the aid of the XML parser

 Registrierung notwendig  SINAMICS XML Parser setup (794,3 KB) 
SHA-256 Checksum: 9604F8D99C682109D6EB3B432A9F6770EB9E654DB003733C0BFE98F0902CB36B

You can find Informations to SHA-256 at the entry
How do you determine the SHA-256 or SHA-512 checksum of a file?

Integrating the warning and error messages into a TIA Portal project (≥V13 SP1)

Integrating the warning and error messages into STEP 7 V5.x / WinCC / WinCC flexible project

Further Information
Inserting error messages of a frequency converter into a WinCC flexible / WinCC (TIA Portal) project 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.