×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 77491575, Entry date: 11/11/2014
(1)
Rate

SINAMICS G120/G120P, CU230P-2: Closed-Loop Control of a tunnel/car park fan

  • Entry
  • Associated product(s)
Application description for the scripted commissioning of a SINAMICS G120 for the control of a tunnel/car park fan
In tunnels and car parks fans and ventilators are used to
  • suction harmful exhausts
  • supply fresh air

In standard operation the volume flow (air) can be closed-loop controlled depending on air quality. In manual mode a fixed fan speed can be adjusted via the motor potentiometer.

Solution
With the function “Hibernate Mode” the converter will be switched off if it is not required for process reasons. With the function “Staging” further fans can be powered up by contactors if a higher volume flow is required. Furthermore a fire operation can be selected. This mode will drive the fan in case of an emergency with an adjustable speed which is independent from the speed control. Fans for both directions of rotation can also be driven by a negative speed setpoint to transport the smoke in a specific direction. In addition to that in fire operation all faults which would not directly switch off the converter will be ignored. Concerning faults which would result in switch-off the converter will be switched on by its automatic restart function after acknowledging all faults.

Picture 01 tunnel fan

Picture 02 car park fan

Note
Commissioning of SIMOTICS FD motors is not supported in this version.
When using load side components as output reactors, dv/dt filters and sinusoidal filters, necessary parameter changes have to be done additional.

Downloads
for SINAMICS G120/G120P, CU230P-2 from FW V4.4
  Documentation (325,2 KB)
 Registrierung notwendig  STARTER Script (8,9 KB) 

Last Changes
02/2014: Script and PDF revised for FW from V4.4
02/2017: Tested with Firmware V4.7 SP6 HF2 and STARTER V4.5.1.0

Additional Keywords
motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.