×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 77491576, Entry date: 11/11/2014
(1)
Rate

SINAMICS G120/G120P, CU230P-2: Closed-Loop Control for a staircase fan

  • Entry
  • Associated product(s)
Application description for the scripted commissioning of a SINAMICS G120 for closed loop control for a staircase fan

Staircases in residential and office buildings are constructed so that they can be ventilated. In the past and still for the most case today this ventilation is effected by windows or at interior, windowless stairwells, by skylights. Depending on the tightness of the cladding especially in the area of the stairwells, windows and doors must be more or less aired by the staircase window.

Solution  
In the application fans for ventilation of staircases are described. In normal operation the fan suctions used air from the stairwell. The speed set point is preset by fixed set points. In addition, a fire mode can be enabled which reverses the direction of rotation of the fan in case of an emergency. This generates a pressure inside the stairwell, so that fire or smoke can not block the escape routes from the floors. The fan speed is controlled by the air pressure. For that reason up to three pressure sensors can be distributed inside the staircase to ensure that even when a door is opened a steady minimum pressure is achieved. In the case of fire faults which would not result in a shutdown of the drive will be ignored. When faults develop which would result in a shutdown the automatic restart will be started and the drive will start again after successful fault acknowledge.

Note
Commissioning of SIMOTICS FD motors is not supported in this version.
When using load side components as output reactors, dv/dt filters and sinusoidal filters, necessary parameter changes have to be done additional.

Downloads
for SINAMICS G120/G120P, CU230P-2 from FW V4.4
  Documentation (289,1 KB)
 Registrierung notwendig  STARTER Script (8,9 KB)

Last Changes
02/2014: Script and PDF revised for FW from V4.4
02/2017: Tested with Firmware V4.7 SP6 HF2 and STARTER V4.5.1.0

Additional Keywords
motioncontrol_apc_applications

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.