×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 775131, Entry date: 06/19/2002
(0)
Rate

Configuring the time synchronization for WinCC clients (WinCC Version < V6.0)

  • Entry
  • Associated product(s)

QUESTION

How do you configure time synchronization for WinCC clients.

ANSWER

  1. Server-client project with non-redundant servers
The clients are synchronized over the system time of the servers. The requirement here is that the computers are in the same network. Configuring the time synchronization is done in four steps:
  • Install the "DCF77Client" tool on all clients that are to be synchronized.
    This software is on the WinCC CD (V4.02 and higher) under "Smart Tools > DCF77Client".
  • After installation start the tool via "Start > Settings > Control Panel > DCF77".
  • In the "Connection" field you must enter the server computer (time master).

 

  • In the Control Panel you must start the "DCF77 receive time signal service" service via the "Services" icon.

    Note

    Make sure that the same time zone is set on both computers.
  1. Server-client project with redundant servers
    Depending on how you have done the time synchronization between the two servers (see Entry ID 622814), you have two options:
  • A separate DCF77 receiver (hardware) is used on the client. This option can however only be used when each of the redundant servers also has a DCF77 receiver (hardware).

    or
  • The time is provided as a project-wide variable on each server. This can then be read out by the client.

Keywords
GMP, Pharma, Life Science, Validation, FDA 21 CFR Part 11

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.