×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 77896780, Entry date: 09/16/2013
(2)
Rate

How do you diagnose an S7-1200 CPU (with CP 1242-7) over the internet/GPRS network?

  • Entry
  • Associated product(s)

Description
Using the "TS Gateway" software supplied with the CP 1242-7 it is possible to diagnose or program an S7-1200 CPU remotely over the internet/GPRS network. For this the PG is connected to the internet over a DSL router. The S7-1200 CPU is connected to a CP 1242-7 that is logged on in the GPRS network.
The figure below shows the configuration for this FAQ response.
More sample configurations are available in the "TS Gateway" system manual in Entry ID 48548898.


Fig. 01

Instructions
The file below contains the instructions for configuring this function and information about it.
 

Contents of the downloads

Download

Configuration instructions ( 1332 KB )

Note
You do not need the "Telecontrol Server Basic" software.
More information on the topic of teleservice using the "Telecontrol Server Basic" software is available in Entry ID 56720905.

Additional Keywords
Remote diagnostics, Remote programming, Remote maintenance

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.