×
Siemens Industry Online Support
Siemens AG
Entry type: FAQ Entry ID: 7808062, Entry date: 09/02/2016
(1)
Rate

What are the requirements for using SIMATIC PDM Data Record Routing?

  • Entry
  • Associated product(s)
This FAQ response gives you information about SIMATIC PDM data record routing and an overview of this ES/AS components supported by PCS 7 for data record routing.

Introduction
Data record routing is a function within SIMATIC S7 modules. SIMATIC PDM uses this function to access parameters and functions of field devices with PROFINET, PROFIBUS DP, PROFIBUS PA and HART communication. SIMATIC PDM is a component of the Engineering Station (ES) and communicates with the automation system (AS) via Ethernet. The AS forwards the request to the field device via PROFINET or PROFIBUS DP. This procedure of data transfer between the plant level and process or field level is called data record routing.

The figure below shows two examples of access options for data record routing from PDM to field devices of the field level.
  


Requirements for data record routing
The automation system must have the interfaces below for data record routing:

  • Ethernet plant bus: CPU/H-CPU with integrated interface or communication processor CP 443-1
  • PROFIBUS DP field bus: CPU with integrated data record gateway or communications processor CP 443-5 Ext

  • PROFINET field bus: PROFINET CPU, H-CPU with integrated data record gateway or communications processor CP 443-1

Note
PROFINET as field bus is supported by PCS 7 V8.0 Upd1 and higher. HART communication is enabled through PROFINET with PCS 7 V8.0 SP1. Check the list of released PROFINET modules.

Note
A list of modules released for a specific version of PCS 7 is available in the entry entitled "Which modules and their firmware versions are released for PCS 7 and how can you upgrade them?" in Entry ID 39709060.
 

1. Interfaces of the Engineering Station (ES)

Data record routing is possible with the ES components below:

HardwareRemark
CP 16136GK1161-3AA00PCI
CP 1613 A26GK1161-3AA01PCI
CP 16236GK1162-3AA00PCI Express
CP 16286GK1162-8AA00PCI Express
Desktop adapter network card (IE General)A5E00718412PCI
A5E01579552PCI Express

 
2. AS comp
onents in PCS 7

PCS 7 supports the following interfaces for data record routing:

  • Communication processors
  • Interfaces of the CPU

Communication processors

Communication processorArticle numberPCS 7
V8.xV7.xV6.xV5.x
CP 443-5 Extended
(PROFIBUS DP)
6GK7 443-5DX02-0XE0 Firmware V3.2 and higherxxxx
6GK7 443-5DX03-0XE0xx
6GK7 443-5DX04-0XE0xx
6GK7 443-5DX05-0XE0x
CP 443-1 EX30 in AS with standard CPU firmware V5.3.1 and higher
(PROFINET)
6GK7 443-1EX30-0XE0x
CP 443-1
(Ethernet)
6GK7 443-1EX02-0XE0xxxx
6GK7 443-1EX10-0XE0xxxx
6GK7 443-1EX11-0XE0xxx
6GK7 443-1EX20-0XE0xx
6GK7 443-1EX30-0XE0x

Interfaces of the CPU
The following versions are possible for data record routing:

  • Standard CPU with PROFIBUS DP Interface firmware V5.1 and higher
  • Standard CPU PN with PROFIBUS DP and PROFINET interface
  • Standard CPU 410-5H Process Automation with PROFIBUS DP and PROFINET interfaces
  • Fault-tolerant CPU (H-CPU) firmware V6.0 and higher with PROFIBUS DP and PROFINET interfaces

Note
More information about using PROFINET components and CPU interfaces in PCS 7 is available in the entry entitled "Which components and controllers can be used to set up a PROFINET field bus in PCS 7?" in Entry ID: 82948099.

The matrix below shows the versions of PCS 7 with which you can use the interfaces of the CPU for data record routing.

PDM data record routing over the interfaces of the CPUStandard CPU
V5.1 and higher
Standard CPU PN
V5.1 and higher
Standard
CPU 410-5H
H-CPU and
H System
V6.0 and higher

WinAC RTX
V4.6 and higher

PCS 7 V8.2YesYesYesYesYes
PCS 7 V8.1YesYesYesYesYes
PCS 7 V8.0 SP1 / SP2YesYes

Yes using the HUP CPU 410-5H from Entry ID 68627630.

YesYes
PCS 7 V8.0YesYesCannot be configuredYesYes
PCS 7 V7.1
including all SPs
YesYesCannot be configuredCannot be configuredCannot be configured
PCS 7 V7.0 SP1 / SP2 / SP3YesYesCannot be configuredCannot be configuredCannot be configured
PCS 7 V7.0Cannot be configuredCannot be configuredCannot be configuredCannot be configuredCannot be configured
PCS 7 V6.1 SP2 / SP3 / SP4YesCannot be configuredCannot be configuredCannot be configuredCannot be configured
PCS 7 V6.1 SP1

Yes using the PCS 7 HSP from Entry ID 26685708

Cannot be configuredCannot be configuredCannot be configuredCannot be configured
PCS 7 V6.1Cannot be configuredCannot be configuredCannot be configuredCannot be configuredCannot be configured
PCS 7 V6.0Cannot be configuredCannot be configuredCannot be configuredCannot be configuredCannot be configured

Note
If the interface of the CPU is used for data record routing, you must configure that CPU with firmware V5.1 or higher in the Hardware Configuration. With an H system or H CPU you must configure the firmware to be V6.0 or higher.

You can use the AS components below for data record routing:

Supported hardware
Y-Link and IM 153 Redundancy BundleNo restrictions
DP/PA Link / IM 157No restrictions
FF LinkCan be configured in PCS7 V8.0 Upd1 and higher and SIMATIC PDM V8.0 SP1
DP/PA couplerEx:6ES7 157-0AD00-0XA0 and successor products
Not Ex: 6ES7 157-0AC80-0XA0 release 3 and higher and successor products
ET 200M6ES7 153-2AA01-0XB0 and successor products
ET 200iSNo restrictions
ET 200iSP (PCS 7 V6.1 and higher)No restrictions
ET 200SPNo restrictions 

Note
See the released modules of your version of PCS 7 in Entry ID: 39709060.

3. Data record routing via IE/PB link

If the combination of CPU and communication processor does not support data record routing, you can use the IE/PB Link as data record gateway. In this way, for example, you can access diagnostics and maintenance data from intelligent field devices and field components over SIMATIC PDM. 

You can use the IE/PB links below for data record routing.

Supported hardware
IE/PB Link 6GK1411-5AA00
IE/PB Link PN IO 6GK1411-5AB00



4. FAQs, application examples and manuals

TitleEntry ID
FAQ - Which requirements have to be fulfilled to perform a STEP 7 routing via a
PG/PC station?
16620173
FAQ - What is the difference between Routing and Data Record Routing?7000978
FAQ - Inter-subnetwork data record routing via a gateway CPU20983154
FAQ - Which modules and their firmware versions are released for PCS 7 and how can you upgrade them?39709060
Application example - Connecting Third-party IOs to PCS 7 via an IE/PB Link PN IO31536572
Manual - Process Device Manager SIMATIC PDM37565982
Function manual - SIMATIC Process Control System PCS 7 Maintenance Station109485949


Additional Keywords

System requirements, Hardware requirements

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.