Entry type: FAQ, Entry ID: 781997, Entry date: 11/29/2010
(0)
Rate

What should I do if the Split Screen Wizard closes with an error message?

  • Entry
  • Associated product(s)


Description

The Split Screen Wizard closes with the following error message:

Possible causes
Probably, when copying the project, you have set the write protection for SSM-relevant (Split Screen Manager) files. Check whether the files in the following directories have the write protection activated:

  • SSM
  • Wscript
  • GraCS
  • Library

You can deactivate the write protection using the DOS command "attrib–r/s" or via the file properties in the Windows Explorer.

Note
The write protection is usually set when you copy the project from a CD to the hard disk.