×
Siemens Industry Online Support
Siemens AG
Entry type: Download Entry ID: 78301954, Entry date: 04/15/2019
(4)
Rate

Firmware Update for the Displays of CPUs 1511(F)/1511C/1512C/1513(F)

  • Entry
  • Associated product(s)
In this entry all firmware version are provided for the displays of CPUs 1511(F)/1511C/1512C/1513(F).

Description:
When updating the firmware, always update to the latest version available for the product and its respective article number. The previous versions of the firmware are only intended as backup to allow a downgrade to the original version. Until now this is not known to have been necessary in any case.
The respective latest version of a firmware is valid for all versions of that article number.

How to update the firmware is described in detail in entry ID 77492231

Overview of article numbers and firmware versions of the displays of CPUs 1511(F)/1511C/1512C/1513(F):

Article number

Firmware version

Update with ...
6ES7591-1AA01-0AA0  
 V2.6.1
Release 04.04.2019

Recommended for update:
For a description, see below Update V2.6.1
 Registrierung notwendig  6ES7591-1AA01-0AA0_V261.ZIP (4,1 MB) 

SHA-256 checksum (Information on SHA-256
 Registrierung notwendig  6ES7591-1AA01-0AA0_V261.txt (1 KB) 

 V2.6.0
Release 12.10.2018 

Backup only:
For a description, see below Update V2.6.0
 Registrierung notwendig  6ES7591-1AA01-0AA0_V260.ZIP (4,1 MB) 

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA01-0AA0_V260.txt (1 KB)

 V2.5.2
Release
06.2018

Backup only:
For a description, see below Update V2.5.2
 Registrierung notwendig  6ES7591-1AA01-0AA0_V252.ZIP (4,1 MB)

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA01-0AA0_V252.txt (1 KB)

 V2.5.1
Release 27.04.2018 

Backup only:
For a description, see below Update V2.5.1
 Registrierung notwendig  6ES7591-1AA01-0AA0_V251.ZIP (4,1 MB)

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA01-0AA0_V251.txt (1 KB)

 V2.5.0
Release 15.12.2017

Backup only:
For a description, see below Update V2.5.0
 Registrierung notwendig  6ES7591-1AA01-0AA0_V250.ZIP (4,1 MB)

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA01-0AA0_V250.txt (1 KB)

 V2.0.0
Release 21.10.2016
Backup only:
For a description, see below Update V2.0.0
 Registrierung notwendig  6ES7591-1AA01-0AA0_V200.ZIP (3,7 MB)
 V1.8.0
Release 09.07.2015
Backup only:
 Registrierung notwendig  6ES7591-1AA01-0AA0_V180.ZIP (3,6 MB) 
   
6ES7591-1AA00-0AA0  
 V2.6.1
Release 04.04.2019

Recommended for update:
For a description, see below Update V2.6.1
 Registrierung notwendig  6ES7591-1AA00-0AA0_V261.ZIP (4,1 MB) 

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA00-0AA0_V261.txt (1 KB) 

 V2.6.0
Release 12.10.2018 

Backup only:
For a description, see below Update V2.6.0
 Registrierung notwendig  6ES7591-1AA00-0AA0_V260.ZIP (4,1 MB) 

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA00-0AA0_V260.txt (1 KB)

 V2.5.2
Release
06.2018

Backup only:
For a description, see below Update V2.5.2
 Registrierung notwendig  6ES7591-1AA00-0AA0_V252.ZIP (4,1 MB)

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA00-0AA0_V252.txt (1 KB)

 V2.5.1
Release 27.04.2018 

Backup only:
For a description, see below Update V2.5.1
 Registrierung notwendig  6ES7591-1AA00-0AA0_V251.ZIP (4,1 MB) 

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA00-0AA0_V251.txt (1 KB)

 V2.5.0
Release 15.12.2017
Backup only:
For a description, see below Update V2.5.0
 Registrierung notwendig  6ES7591-1AA00-0AA0_V250.ZIP (4,1 MB)

SHA-256 checksum (Information on SHA-256)
 Registrierung notwendig  6ES7591-1AA00-0AA0_V250.txt (1 KB)
 V2.0.0
Release 21.10.2016
Backup only:
For a description, see below update V2.0.0
 Registrierung notwendig  6ES7591-1AA00-0AA0_V200.ZIP (3,7 MB) 
 V1.8.0
Release 09.07.2015

Backup only:
For a description, see below Update V1.8.0
 Registrierung notwendig  6ES7591-1AA00-0AA0_V180.ZIP (3,6 MB)

 

V1.7.0
Release 23.12.2014

Backup only:
For a description, see below Update V1.7.0
 Registrierung notwendig  5911AA00_V170.EXE (3,7 MB)

 

V1.6.0
Release 07.08.2014

Backup only:
For a description, see below Update V1.6.0
 Registrierung notwendig  5911AA00_V160.EXE (3,1 MB)

 

V1.5.0
Release 28.02.2014

Backup only:
For a description, see below Update V1.5.0
 Registrierung notwendig  5911AA00_V150.EXE (3,2 MB)

 

V1.1.0
Release 26.07.2013

Backup only:
For a description, see below Update V1.1.0
 Registrierung notwendig  5911AA00_V110.EXE (5,9 MB)

 

V1.0.1
Release 27.02.2013

Backup only:
 Registrierung notwendig  5911AA00_V101.EXE (6,2 MB)


Update V2.6.1 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

You can find details on firmware version V2.6.1 in the entry Firmware-Update S7-1500 CPUs incl. Displays und ET 200 CPUs (ET 200SP, ET 200pro)  


Update V2.6.0 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

You can find details on firmware version V2.6.0 in the entry Firmware-Update S7-1500 CPUs incl. Displays und ET 200 CPUs (ET 200SP, ET 200pro)  


Update V2.5.2 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

Change caused by production.


Update V2.5.1 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

You can find details on firmware version V2.5 in the entry Firmware-Update S7-1500 CPUs incl. Displays und ET 200 CPUs (ET 200SP, ET 200pro)  

 

Update V2.5.0 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

You can find details on firmware version V2.5 in the entry Firmware-Update S7-1500 CPUs incl. Displays und ET 200 CPUs (ET 200SP, ET 200pro)


 
Update V2.0.0 (6ES7591-1AA00-0AA0 and 6ES7591-1AA01-0AA0)

New features with firmware V2.0:

  • After activating the option "Configuration control (option handling)“ in the engineering, an indicator is output on the display.
  • "Online backup and restore“ via the display in the CPU STOP condition, that means the content of the SIMATIC memory card and the remanent data of the CPU can be stored directly via the display. The file is stored on the SIMATIC memory card. Via "Restore“, data stored online on the memory card can be loaded onto the CPU.
  • The "Read-Only“ default for the display can be set in the engineering.
  • The SIMATIC memory card can be formatted via the display.
  • The project name of the TIA Portal project loaded onto the CPU is shown on the display.
  • Acknowledgment of messages directly on the display
  • On the display, variables can be directly displayed respectively changed via the absolute address.

 

Update V1.8.0 (6ES7591-1AA00-0AA0)

New features available with firmware V1.8

  • Writing access to variables in a variables table via the display
  • The information “know how protected“ will only be displayed if password-protected user blocks are being used in the program.

 

Update V1.7.0 (6ES7591-1AA00-0AA0)

New features available with firmware V1.7

  • Indication, whether there are know-how protected software blocks in the CPU
  • Indication, whether the copy protection for program blocks has been activated in the CPU
  • Fast scrolling in the display if the cursor key is held down.
  • Usability improvements when setting the daylight saving time and the IP settings

 

The following problems have been corrected:

  • The page number on the display is indicated correctly.
  • In the case of Korean diagnostic texts the characters will now be represented correctly.


Update V1.6.0 (6ES7591-1AA00-0AA0)

New features with firmware V1.6

  • Scaled indication of the available memory / used memory / free memory
  • Indication of the CPU cycle time (minimum, maximum, latest) on the display
  • The absolute address and the commentary of the relevant variables are indicated on the display in monitoring tables.

Update V1.5.0 (6ES7591-1AA00-0AA0)

New features with firmware V1.5

  • The IP-address of the integrated CPU interface is displayed on the starting screen,
  • Additional overview page on displays with 3.45cm screen diagonal to indicate information such as IP-address of the integrated interface or the FW version.
  • Russian, Turkish, Japanese, Portuguese and Korean added to the user interface languages of the displays
  • A user-defined logo can be inserted on the display
  • Automatic update for the diagnostic buffer and message indication on the display
  • Change of the time zone setting on the display
  • If write protection has been activated for the SIMATIC Memory Card this will be indicated on the display
  • Reading access to configured force and variable tables
  • The IP-addresses of the connected Ethernet CPs can be set via the display.

Update V1.1.0 (6ES7591-1AA00-0AA0)

The following new functions have been implemented:

  • Enhanced performance of the operator input
  • The "Links Key" can be used to fade in Tooltips at many places
  • Additional diagnostic information with respect to the SIMATIC Memory Card: no card inserted, FW update card is inserted, error indication if no project is loaded
  • During the download process via the TIA Portal the display indicates that a download is in progress
  • When you press the "ESC" button for more than 3 secs. there will be an automatic jump to the starting page.


 

Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
http://www.siemens.com/industrialsecurity.