×
Siemens Industry Online Support
Siemens AG
Entry type: Application example Entry ID: 78346833, Entry date: 05/21/2019
(54)
Rate

Installation and operation of WinCC in a Microsoft domain environment

  • Entry
  • Associated product(s)
This tutorial shows you how to set up a domain server and add or remove domain clients to or from a domain. Furthermore, you will be shown how to install WinCC V7/V15 Professional on a domain client and what you have to consider during operation and installation.

The task
Complex IT infrastructure networks with domain controllers are used in many areas of industrial and manufacturing facilities.
A domain controller is a server used to centrally manage computers or users. In this way, a lot of time and effort is saved during operation and maintenance of the system.

WinCC V7/V15 Professional is to be used on a computer that is a member of a domain.

Solution
Due to the complex IT infrastructure networks in many areas of industrial and manufacturing plants, this configuration guide covers two main scenarios of installation and operation of WinCC V7/V15 Professional.

  • Installation on a computer already integrated in the domain.
  • Installation on a computer outside the domain with subsequent integration into the domain.


 

Advantages
This application offers you the following advantages:

  • Low training effort for the domain installation of WinCC, thus low installation and configuration effort for implementing your own configuration.
  • Detailed description of the operation of WinCC V7/V15 Professional in one domain, thus fast build-up of know-how.
  • A manual for configuring the Windows operating system with recommended and tested settings for error-free commissioning and stable operation.

Downloads
  Installation and Operation of WinCC in a Domain with Microsoft Server Operating System (2,2 MB)

Operation on network servers
It is not permitted to operate WinCC on network servers (e.g. domain controllers, file and name utility servers, routers, software firewalls, media servers, exchange servers, etc.).


Additional keywords
Workgroup, domain member, domain name, domain controller, domain, hostname, access rights in SIMATIC WinCC, SIMATIC HMI CS, SIMATIC HMI VIEWER, DM_USER, DM_ADMIN, DNS name resolution, DNS server, LAN connection, TCP/IP, static fixed IP address, Active Directory Domain Services, DNS suffix, NetBIOS, AD DS, 60605851 


Security information
In order to protect technical infrastructures, systems, machines and networks against cyber threats, it is necessary to implement – and continuously maintain – a holistic, state-of-the-art IT security concept. Siemens’ products and solutions constitute one element of such a concept. For more information about cyber security, please visit
https://www.siemens.com/cybersecurity#Ouraspiration.
Rate entry
no rating
Requests and feedback
What do you want to do?
Note: The feedback always relates to the current entry / product. Your message will be forwarded to our technical editors working in the Online Support. In a few days, you will receive a response if your feedback requires one. If we have no further questions, you will not hear from us.